2022-07-01 02:22 AM
2022-07-08 05:53 AM
Hello @LJIAN.1 ,
Thanks for your feedback,
Could you please specify the CubeMX version and which OS are you using ?
Sara.
2022-08-16 05:58 PM
I have the same problem, and I use the latest CubeMX. I run this software in windows10.
2022-08-16 08:17 PM
2022-08-16 08:27 PM
thank you.
2022-08-16 11:32 PM
Hi @LJIAN.1 and @AlgoOy ,
Can you give us the Wind10 PC HW config:
Can you also monitor your available PC RAM availability when you observe this issue, I guess RAM availability issue.
Can you confirm that this behavior is systematic even with a PC reboot ?
Regards,
Aymen.
2022-08-16 11:46 PM
CPU:
AMD Ryzen 7 5800H with Radeon Graphics
Base speed: 3.20 GHz
GPU:
NVIDIA GeForce RTX 3070 Laptop GPU
Driver version: 31.0.15.1694
Memory:
32.0 GB
Speed: 3200 MHz
Available 16.4 GB
In use (Compressed) 11.4 GB (467 MB)
PC Model:
Legion R9000P2021H
Processor AMD Ryzen 7 5800H with Radeon Graphics 3.20 GHz
Installed RAM 32.0 GB (27.9 GB usable)
This kind of situation happened every time, and even if I restart the computer.
2022-09-11 07:38 PM
I have the same problem too !!
2022-09-14 05:00 AM
I have the same problem too !!
2022-10-24 06:14 PM
I have the same problem too !!