2014-07-06 06:59 AM
Hi guys,
I tried to make a project by STM32CubeMX. I configured the MCU and the Project file is this (USART.ioc) :#MicroXplorer Configuration settings - do not modify
#Sun Jul 06 17:52:14 IRDT 2014
File.Version=4
KeepUserPlacement=false
Mcu.Family=STM32F0
Mcu.IP0=NVIC
Mcu.IP1=RCC
Mcu.IP2=USART1
Mcu.IPNb=3
Mcu.Name=STM32F030F4Px
Mcu.Package=TSSOP20
Mcu.Pin0=PF0-OSC_IN
Mcu.Pin1=PF1-OSC_OUT
Mcu.Pin2=PA0
Mcu.Pin3=PA2
Mcu.Pin4=PA3
Mcu.PinsNb=5
Mcu.UserName=STM32F030F4Px
NVIC.EXTI0_1_IRQn=true\:0\:0
NVIC.SysTick_IRQn=true\:0\:0
NVIC.USART1_IRQn=true\:0\:0
PA0.GPIOParameters=GPIO_PuPd,GPIO_ModeDefaultEXTI
PA0.GPIO_ModeDefaultEXTI=GPIO_MODE_IT_RISING
PA0.GPIO_PuPd=GPIO_PULLDOWN
PA0.Locked=true
PA0.Signal=GPXTI0
PA2.Mode=Asynchronous
PA2.Signal=USART1_TX
PA3.Mode=Asynchronous
PA3.Signal=USART1_RX
PCC.Family=STM32F0
PCC.MCU=STM32F030F4Px
PCC.MXVersion=4.3.0
PCC.PartNumber=STM32F030F4Px
PCC.Seq0=0
PCC.SubFamily=STM32F030 Value Line
PCC.Temperature=25
PCC.Vdd=3.6
PF0-OSC_IN.Mode=HSE-External-Oscillator
PF0-OSC_IN.Signal=RCC_OSC_IN
PF1-OSC_OUT.Mode=HSE-External-Oscillator
PF1-OSC_OUT.Signal=RCC_OSC_OUT
ProjectManager.AskForMigrate=true
ProjectManager.BackupPrevious=false
ProjectManager.CompilerOptimize=2
ProjectManager.ComputerToolchain=false
ProjectManager.CoupleFile=false
ProjectManager.DeletePrevious=true
ProjectManager.DeviceId=STM32F030F4Px
ProjectManager.FirmwarePackage=STM32Cube FW_F0 V1.0.0
ProjectManager.FreePins=false
ProjectManager.HalAssertFull=false
ProjectManager.KeepUserCode=true
ProjectManager.LastFirmware=true
ProjectManager.LibraryCopy=0
ProjectManager.ProjectBuild=false
ProjectManager.ProjectFileName=USART.ioc
ProjectManager.ProjectName=USART
ProjectManager.TargetToolchain=MDK-ARM 4.73
RCC.FamilyName=M
RCC.IPParameters=PLLSource,PLLMUL,FamilyName,SYSCLKSource
RCC.PLLMUL=RCC_PLL_MUL6
RCC.PLLSource=RCC_PLLSOURCE_HSE
RCC.SYSCLKSource=RCC_SYSCLKSOURCE_PLLCLK
SH.GPXTI0.0=GPIO_EXTI0
SH.GPXTI0.ConfNb=1
USART1.BaudRate-Asynchronous=921600
USART1.IPParameters=BaudRate-Asynchronous
Am I right?
I want to use interrupte for send and recive the data.
my next question is:
after configure the peripherals and MCU via STM32CubeMX, should I configure the project files manualy? I want to use the functions (or APIs) of UART header file but I don't know how!
for example, should I use these both functions?:
HAL_StatusTypeDef HAL_UART_Transmit_IT(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size);
HAL_StatusTypeDef HAL_UART_Receive_IT(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size);
How can I use those functions? should I handle anything?
#uart #stm32cubemx
2014-08-06 05:09 AM
Hi Brian,
You have to compile the generated project in order to check if it is OK. Then you have to add your own code depending on your use case. You can refer to the USART examples in the Cube package to have an idea about the other updates to do. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.