2021-11-23 3:14 AM
I m trying to configure the ADC1 in DMA modality with STM32F303K8
when I debug the values does not change at all.
With the breakpoint i could see that DMA1_Channel1_IRQHandler is called.
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim2;
TIM_HandleTypeDef htim3;
UART_HandleTypeDef huart1;
/* USER CODE BEGIN PV */
int32_t enc_value1;
int32_t enc_value2;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM2_Init(void);
static void MX_TIM3_Init(void);
static void MX_USART1_UART_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
int32_t Count1=0;
int32_t Count2=0;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_TIM2_Init();
MX_TIM3_Init();
MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_Encoder_Start_IT(&htim2, TIM_CHANNEL_ALL);
HAL_TIM_Encoder_Start_IT(&htim3, TIM_CHANNEL_ALL);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}void DMA1_Channel1_IRQHandler(void)
{
/* USER CODE BEGIN DMA1_Channel1_IRQn 0 */
/* USER CODE END DMA1_Channel1_IRQn 0 */
HAL_DMA_IRQHandler(&hdma_adc1);
/* USER CODE BEGIN DMA1_Channel1_IRQn 1 */
/* USER CODE END DMA1_Channel1_IRQn 1 */
}
Solved! Go to Solution.
2021-11-23 5:25 AM
The DMA initialization MX_DMA_Init(); should be before other peripheral initialization.
2021-11-23 4:04 AM
Hello @FTrom ,
You are missing the DMA initialization MX_DMA_Init(); which should be before other peripheral initialization.
Please try this, then let me know if this solved your issue, if so please "Select as Best" button.
Imen
2021-11-23 4:31 AM
Hi Imen
if I understand correctly I should modify as
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_DMA_Init();
MX_ADC1_Init();But unfortunately, the values are stoked as before
Thanks
2021-11-23 5:14 AM
The code you posted in the OP doesn't initialize the ADC or the DMA.
2021-11-23 5:25 AM
The DMA initialization MX_DMA_Init(); should be before other peripheral initialization.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.