cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-LPM01A installation issue

paolog
Associate III

Hi!

I'm having problem connecting the board to a Windows 10 PC. Connecting the board to the USB it works in standalone mode, but the USB driver (PowerShield Virtual ComPort in FS Mode) is not installed, so I can't use the board with the STM32CubeMonitor-Power. Windows Device Manages tells that device drivers have not been installed, and the associated COM port is obviously not existing.

Is the X-NUCLEO-LPM01A not functioning properly or am I missing something?

1 ACCEPTED SOLUTION

Accepted Solutions
paolog
Associate III

Ok, I just needed to upgrade the firmware of the X-NUCLEO-LPM01A...

View solution in original post

1 REPLY 1
paolog
Associate III

Ok, I just needed to upgrade the firmware of the X-NUCLEO-LPM01A...