2023-10-24 07:06 AM
I have installed STM32 Cube Monitor Power on Debian 12 (64 bit) and have connected a LPM01A via USB. When I run the power monitor, no board shows up in the drop down menu. I have tried the two versions of the power monitor available on the ST website.
Running lsusb, I can see a device called `STMicroelectronics Virtual COM Port`, which corresponds to the LPM01A.
How can I get the power monitor to connect to the LPM01A?
2023-12-04 01:14 AM
Hello,
As indicated in User Manual UM2202 (chapter 2.1), supported operating systems include Linux, but only distributions Red Hat, Fedora, and Ubuntu, has been tested.
We recommand to use these distributions.
Regards