2023-08-14 8:09 AM - edited 2023-08-14 8:09 AM
Hello,
I'm using the current version of STM32CubeMonitor (1.6.0) under Windows and would like to check in my flow if the configured exefile in the STMicroelectronics variable node is the intended one (e.g fits a regex). For this I would like to read out the exefile parameter. Using a debug-node I can see it is written but 'undefined'.
Is there a workaround for this or is it possible to give the exefile as input parameter to the variable node?
My output looks like this:
object
groupname: "STM32G0 Binary Production"
variablelist: array[19]
mode: "direct"
snapshotheader: ""
triggerstartmode: "manual"
triggername: "my_unused_variable"
triggerthreshold: ""
frequency: 10
accesspoint: 0
exefile: undefined
Thank you!
Solved! Go to Solution.
2023-09-07 2:32 AM
Hello @MKori.1
The fact that exefile appears as undefined is a known bug that will be fixed in next 1.7.0 release planned in a short term.
2023-08-31 7:45 AM
Hello @MKori.1,
I'm afraid, it's not possible to give exe file as input parameter of the variable node. May be you can try a solution using regexp-filter in order to verify your file.
2023-08-31 8:01 AM
Hello @Richard.Chvr ,
thank you for your response. Yes, this together with a .json parser this is my current solution. It has some drawbacks, for instance when mulitple exefile configurations are defined checking the correct one is some additional effort.
What is about the empthy "exefile" output of the node? Is there some information output planned?
2023-09-07 2:32 AM
Hello @MKori.1
The fact that exefile appears as undefined is a known bug that will be fixed in next 1.7.0 release planned in a short term.