cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMonitor stuck at 10% when parsing .elf

_kj_
Associate

When compiling with Maximum (-g3) Debug level, Add new exe-config config mode stalls at 10% when loading .elf. Why is this? Is there a limit to the number of symbols or the size of the .elf?

If compiled with Default (-g) Debug level, then loads OK.

When the project was simpler, fewer files, it did load OK with-g3 Debug level.

STM32 CubeMonitor version 1.6.0     Windows 11
GNU Tools for STM32 (10.3-2021.10)

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Richard.Chvr
ST Employee

Hello @_kj_ 

What is the size of your elf file? Can you share it?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.