2020-04-07 2:58 AM
Hi,
I would like to set the minimum and maximum values of a dashboard chart using custom values calculated with a processing node.
I tried "single value" and "change" nodes, but without success.
I attached my current flow...
Thank you
Walter
Solved! Go to Solution.
2022-09-29 11:44 PM
I'm also supporting this idea! Manually setting the limits of the chart would be very helpful in quite a few cases. Are there any current plans to include this functionality?
Don't get me wrong: Autoscaling is helpful very often. But sometimes it is not...
2025-01-09 2:13 AM
@Thierry
Any news on the state of implementation of this?
I noticed that the chart's help shows that there's a property "Y-Axis" where one can manually set the limits but I cannot see this property in the actual chart settings.
2025-01-30 5:59 AM
Hello @DMeie.2 .
"Y-Axis" property is only available for Bar Chart type.