cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.16.0 released

Semer CHERNI
ST Employee

STM32CubeIDE 1.16.0 was released today on st.com as well as an in-tool update patch.

  • What is new in 1.16.0?
    • Microcontroller and board lists aligned with STM32CubeMX v6.12.0 : STM32C0 ,STM32WB0 and STM32MP25XX
    • Added CMake support for multicontext projects (Multi-Context ,Trust zone , Multi-core)
    • Added new features for CMake project configuration
    • Basic CMake support now also with Ninja
    • Added the OZ in the optimization level to the build settings
  • Main fixed issues:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Known issues fixed and problems and limitations:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Where do I obtain STM32CubeIDE 1.16.0?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

0 REPLIES 0