cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.15.0 released

Semer CHERNI
ST Employee

STM32CubeIDE 1.15.0 was released today on st.com as well as an in-tool update patch.

  • What is new in 1.15.0?
    • Microcontroller and board lists aligned with STM32CubeMX v6.11.0 : STM32U0, STM32H7Rx/STM32H7Sx and STM32H523/STM32H533
    • Added the support for the Q-Format in the Live Expressions view
    • Added the support for Arm® Cortex®‑A7 registers in the SFRs view
    • Switched to GCC 12 as a default toolchain
    • Added the support for Fedora® 37 and macOS 14 (Sonoma)
    • Updated to Eclipse® 2023-12
  • Main fixed issues:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Known issues fixed and problems and limitations:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Where do I obtain STM32CubeIDE 1.15.0?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

0 REPLIES 0