2023-05-15 06:58 AM - edited 2023-11-20 05:26 AM
2023-05-15 07:49 AM
Hello @DShet.2 and welcome to the community,
Could you, please, share the steps that you followed to change the dark theme or if you have changed something else . In fact, I couldn't reproduce this issue.
Thanks,
Rim.
2023-05-15 08:13 AM - edited 2023-11-20 05:26 AM
Correction: The text is fine only with Theme: Classic. The text is seems to be broken in "Light" Mode too
Here are the steps:
Windows-> Preference->General->Appearance->Theme:Dark.
The above image shows theme:Classic(WORKS FINE HERE)
The above image shows theme: Light
The above image shows theme:Dark.
PS: The restart prompt don't matter. I have restarted the PC, IDE. Also tried re-installing. Nothing works.
2023-05-16 03:21 AM
Weird! What host computer OS and language configuration are you using? and what is the App display language? Is this the first time you've encountered this problem with CubeIDE version 1.12.1?
Any additional information would be appreciated!
2023-10-09 06:35 PM
Apologies for reviving an old thread, but I'd very much like to get an answer for this as well.
I encountered this issue on a fresh install of CubeIDE version 1.13.1. I haven't used any previous versions of the software. I'm using whatever the most recent 64-bit windows version was, and my system language is set to English (Australia). I have the exact same issue where dark and light mode result in unreadable tab titles, but classic mode displays just fine. Below are snips of the same sub-window in dark, light, and classic themes respectively.
2023-10-10 03:08 AM
Hello @McNubby ,
I am sorry but the issue is not reproduced using STM32CubeIDE 1.13.1 on 64-bit windows machine.
Is there any other configuration made under preferences?
Thanks,
Rim
2024-08-25 07:56 AM
I have the same issue in STM32CubeIDE too, but I also have it on STM32CubeProgrammer (this is a fresh install)
Also, my computer language is set to English(US)