2024-04-14 8:29 PM
Hello,
I just created a new project and want to use TIM5 in encoder mode, but I can't due to the following error.
How can I solve this?
Thank you for your assistance.
Solved! Go to Solution.
2024-04-14 9:28 PM
Hello @HMsDobby2
I suggest you put the cursor on the option the option that you want to know why you can't select it. A pop-up will appear with a message that tels you why this option is not available and what you should do to select it if possible. You can also add the board/MCU that you are using here so we can check.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-14 9:28 PM
Hello @HMsDobby2
I suggest you put the cursor on the option the option that you want to know why you can't select it. A pop-up will appear with a message that tels you why this option is not available and what you should do to select it if possible. You can also add the board/MCU that you are using here so we can check.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-14 9:41 PM
I managed to solve the problem by checking the error message that way. Thank you!