cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I find v1.14.1 for generic linux, debian and mac?

PHolt.1
Senior III

On the ST website it shows 1.14.0 and 1.15.0 and 1.15.1.

But also if I try to download the 1.14.0, say generic linux, I just get the debian one every time 

en.st-stm32cubeide_1.14.0_19471_20231121_1200_amd64.deb_bundle.sh.zip

I need the above to archive my project. v1.15.0 broke some stuff so I have up on it and finished with 1.14.1.

The windows 1.14.1 I have OK.

Any help much appreciated.

 

1 ACCEPTED SOLUTION

Accepted Solutions
Mahmoud Ben Romdhane
ST Employee

Hello @PHolt.1 ,

First let me thank you for posting.

The STM32CubeIDE 1.14.1 is supported only on windows in order to resolve the issue with Prebuild or Postbuild commands.

I suggest that you take a look at the RN0114 section 3.3 STM32CubeIDE v1.14.1 release information.

Thanks.

Mahmoud.

View solution in original post

3 REPLIES 3
Mahmoud Ben Romdhane
ST Employee

Hello @PHolt.1 ,

First let me thank you for posting.

The STM32CubeIDE 1.14.1 is supported only on windows in order to resolve the issue with Prebuild or Postbuild commands.

I suggest that you take a look at the RN0114 section 3.3 STM32CubeIDE v1.14.1 release information.

Thanks.

Mahmoud.

PHolt.1
Senior III

Thank you. I downloaded 1.14.0 of the three versions.

 

PHolt.1
Senior III

Does ST publish hashes for its install packages, enabling one to check whether an archived (say) Cube IDE 1.14.1 has been modified or not?