cancel
Showing results for 
Search instead for 
Did you mean: 

what causes these libc_nano.a errors?

carlesls2
Associate III

Description Resource Path Location Type
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v6-m/nofp\libc_nano.a(libc_a-closer.o): note: the message above does not take linker garbage collection into account RA40 C/C++ Problem
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v6-m/nofp\libc_nano.a(libc_a-lseekr.o): note: the message above does not take linker garbage collection into account RA40 C/C++ Problem
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v6-m/nofp\libc_nano.a(libc_a-readr.o): note: the message above does not take linker garbage collection into account RA40 C/C++ Problem
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v6-m/nofp\libc_nano.a(libc_a-writer.o): note: the message above does not take linker garbage collection into account RA40 C/C++ Problem
_close is not implemented and will always fail RA40 C/C++ Problem
_lseek is not implemented and will always fail RA40 C/C++ Problem
_read is not implemented and will always fail RA40 C/C++ Problem
_write is not implemented and will always fail RA40 C/C++ Problem

 

 

What causes this error? I do not know why or when it apeared and how to erase it. 

Thanks for all. 

 

1 ACCEPTED SOLUTION

Accepted Solutions

@Andrew Neil wrote:

I think that the messages you have there are just warnings - not errors?


Indeed they are - see:

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-13-0-problem/m-p/573904/page/3

"this is ‘just’ a warning, and the linker is able to generate a proper ELF file. As long as your application does not use read/write/close/lseek (which should be the case for a bare metal application), your application will run properly."

 

Also, I think that CubeIDE only produces these warning on the very first build of a new project - they don't appear in subsequent builds?

View solution in original post

5 REPLIES 5

I can't read that image!

Please copy & paste the messages at text.


OP has been changed - now it's just the text, no image.

Please don't edit a post after it's had replies - especially when it means existing replies no longer make sense!

Those messages seem to be in the wrong order; eg, the first one refers to "the message above".

That's the trouble with CubeIDE's  'Problems' view - it reorders the message.

So best to copy from the 'Console' view.

Sorry - forgot to mention that this time:

https://community.st.com/t5/stm32cubeide-mcus/stmcubeide-generating-errors-in-the-driver-files-on-creation-of/m-p/97912/highlight/true#M2765

 

But I think that the messages you have there are just warnings - not errors?

 

TDK
Guru

Please see answer here:

Solved: Cube IDE 1.15.0 - STMicroelectronics Community

If you feel a post has answered your question, please click "Accept as Solution".

That thread relates to CubeIDE v1.15.0, and says it should have been fixed, "on the next releases".

@carlesls2 What version are you using?

@STTwo-32 did it get fixed?

 

PS:

From the pathnames in @carlesls2's  OP, looks like v1.18.0 ...


@Andrew Neil wrote:

I think that the messages you have there are just warnings - not errors?


Indeed they are - see:

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-13-0-problem/m-p/573904/page/3

"this is ‘just’ a warning, and the linker is able to generate a proper ELF file. As long as your application does not use read/write/close/lseek (which should be the case for a bare metal application), your application will run properly."

 

Also, I think that CubeIDE only produces these warning on the very first build of a new project - they don't appear in subsequent builds?