2025-03-24 2:35 AM - last edited on 2025-03-24 3:17 AM by Andrew Neil
Description Resource Path Location Type
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v6-m/nofp\libc_nano.a(libc_a-closer.o): note: the message above does not take linker garbage collection into account RA40 C/C++ Problem
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v6-m/nofp\libc_nano.a(libc_a-lseekr.o): note: the message above does not take linker garbage collection into account RA40 C/C++ Problem
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v6-m/nofp\libc_nano.a(libc_a-readr.o): note: the message above does not take linker garbage collection into account RA40 C/C++ Problem
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v6-m/nofp\libc_nano.a(libc_a-writer.o): note: the message above does not take linker garbage collection into account RA40 C/C++ Problem
_close is not implemented and will always fail RA40 C/C++ Problem
_lseek is not implemented and will always fail RA40 C/C++ Problem
_read is not implemented and will always fail RA40 C/C++ Problem
_write is not implemented and will always fail RA40 C/C++ Problem
What causes this error? I do not know why or when it apeared and how to erase it.
Thanks for all.
Solved! Go to Solution.
2025-03-24 6:10 AM
@Andrew Neil wrote:I think that the messages you have there are just warnings - not errors?
Indeed they are - see:
https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-13-0-problem/m-p/573904/page/3
"this is ‘just’ a warning, and the linker is able to generate a proper ELF file. As long as your application does not use read/write/close/lseek (which should be the case for a bare metal application), your application will run properly."
Also, I think that CubeIDE only produces these warning on the very first build of a new project - they don't appear in subsequent builds?
2025-03-24 2:54 AM - edited 2025-03-24 3:11 AM
I can't read that image!
Please copy & paste the messages at text.
OP has been changed - now it's just the text, no image.
2025-03-24 3:17 AM
Please don't edit a post after it's had replies - especially when it means existing replies no longer make sense!
Those messages seem to be in the wrong order; eg, the first one refers to "the message above".
That's the trouble with CubeIDE's 'Problems' view - it reorders the message.
So best to copy from the 'Console' view.
Sorry - forgot to mention that this time:
But I think that the messages you have there are just warnings - not errors?
2025-03-24 5:59 AM
Please see answer here:
Solved: Cube IDE 1.15.0 - STMicroelectronics Community
2025-03-24 6:03 AM - edited 2025-03-24 6:04 AM
That thread relates to CubeIDE v1.15.0, and says it should have been fixed, "on the next releases".
@carlesls2 What version are you using?
@STTwo-32 did it get fixed?
PS:
From the pathnames in @carlesls2's OP, looks like v1.18.0 ...
2025-03-24 6:10 AM
@Andrew Neil wrote:I think that the messages you have there are just warnings - not errors?
Indeed they are - see:
https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-13-0-problem/m-p/573904/page/3
"this is ‘just’ a warning, and the linker is able to generate a proper ELF file. As long as your application does not use read/write/close/lseek (which should be the case for a bare metal application), your application will run properly."
Also, I think that CubeIDE only produces these warning on the very first build of a new project - they don't appear in subsequent builds?