2023-06-11 12:54 AM
Hi,
Trying to get he new STM32 Extension working for VS Code and it is failing with
> Using vcpkg executable at "/home/iwiseman/.vscode/extensions/ms-vscode.vscode-embedded-tools-0.7.0-linux-x64/assets/platform/linux-x64/vcpkg-glibc.app".
> Using VCPKG_ROOT at "/home/iwiseman/.config/Code/User/globalStorage/ms-vscode.vscode-embedded-tools/vcpkg/root".
> Activating environment at "/home/iwiseman/dev/stm32cubeide-workspace/Test6/vcpkg-configuration.json".
> Version of vcpkg used to create VCPKG_ROOT: "2023-04-07-bedcba5172f5e4b91caac660ab7afe92c27a9895".
> Running vcpkg with arguments ["version"].
vcpkg package management program version 2023-03-14-105f7f7e8a5ea10dfac9874ff9d1a6bacba5f454
See LICENSE.txt for license information.
> Bundled version of vcpkg: "2023-03-14-105f7f7e8a5ea10dfac9874ff9d1a6bacba5f454".
> Versions do not match. Reinstalling vcpkg.
> Running vcpkg with arguments ["bootstrap-standalone"].
Downloading standalone bundle 2023-03-14.
> Running vcpkg with arguments ["activate","--project","/home/iwiseman/dev/stm32cubeide-workspace/Test6","--json","/tmp/dbd870692f4d83c38db7324385cbdaa0"].
warning: vcpkg-artifacts is experimental and may change at any time.
Downloading vcpkg-artifacts bundle 2023-03-14...
error: Failed to provision vcpkg-artifacts.
> Failed with exit code "1".
> Failed to activate environment at "/home/iwiseman/dev/stm32cubeide-workspace/Test6/vcpkg-configuration.json".
I have tried
Happy to share logs run tests etc. Just want my stuff to work.
Using
Ubuntu 23.04
VS Code 1.79.0
stm32CubeIDE 1.12.1
I have not installed anything specific except
CMake
Nigja build
Build Essential
Thanks,
2023-06-11 4:41 AM
Guessing this is the problem. https://github.com/microsoft/vcpkg/issues/30474
Will investigate when work allows and feedback.
Want to spend sometime using the boards instead of getting software to work.
2023-06-12 12:16 AM - edited 2023-11-20 3:29 AM
So add the setting for vs code
"vcpkg.diagnostics.additionalArguments": [ "--debug" ]
Lots of debug and it did fail. But I did notice it was looking in /home/iwiseman/.cache/vcpkg. Removing this and retrying still did not work but need I went to extensions for embedded and installed pre-release
It did not work straight away but removing the vcpkg directory again and it did succeed.
I now have an .elf .bin and .hex file.
Next is uploading and debugging.
2023-11-12 10:53 AM
Worked for me: execute the vscode command (Ctrl-Shift P) vcpkg: Activate vcpkg environment
Overall it seems coming from a deficiency of ms-vscode.vscode-embedded-tools