2024-05-20 10:02 PM - edited 2024-05-20 10:06 PM
Hi ,
I was given by a task to connect an external load to STM32L562 for USBPD. Do you guys have any idea how to start and what to do in the inital process.
Task details
Support all 100W+ USB PD EPR power profiles using standard USB PD 3.1 parameters, 100W (20V @ 5A), 140W (28V @ 5A) , 180W (36V @ 5A) , 240W (48V @ 5A). 240W may not be able to be tested during this phase due to market availably of OTS 240W supplies, however functionality should be added for future use
Requires an external load on the module connectors to validate power delivery output capability
Solved! Go to Solution.
2024-05-21 05:25 AM
Hi @nishadh
TCPP upgrade to support EPR voltages is ongoing
For further details, check this thread Solved: Re: USB PD sink - STMicroelectronics Community
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-21 05:25 AM
Hi @nishadh
TCPP upgrade to support EPR voltages is ongoing
For further details, check this thread Solved: Re: USB PD sink - STMicroelectronics Community
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.