cancel
Showing results for 
Search instead for 
Did you mean: 

Terrible horrific problems with CubeIDE 1.17. I am SAD.

JerryMC22
Associate II

Hi boys and girls from ST company - capitalistic USA country,

 

I installed your new CubeIDE 1.17 today and I ascertained that:

1/ If I open a project everything is closed - no window is visible. If I try to close the project, the project is NOT closed and moreower I can even COMPILE !!! and debug and to programm the closed project :) It is very cute.

Whe I was very young we had a car "Škoda MB100" (green color). It was very magic car. If there were lack of water in the main cooler and if the car engine was hot enough e.g. approx. 100°C I could remove the ignition key from ignition box, but the car engine runs gaily without stopping :)   :) :) :) :)  And this situation continued even if I removed the car battery 12V/64Ah :) :) :) :)  YES !!!

 

2/ I tried to change dark gray text color background in C/C++ editor and ... surprisingly ...  it is NOT possible. See video here: 

https://cloud.fastshare.cz/share/get/t51aVjDx2LKVKJ8U3q9YqvJMtKaUDrHlkmttGhkdNNjsRP5mj2xPk6Y3Ti8EHcK8 

It is very cute situation. (download is free of charge)

Can you please repair ALL problems ?

Many thanks

Jerry

 

4 REPLIES 4
TDK
Guru

Duplicate of this post:

CubeIDE problems - STMicroelectronics Community

 

> If I open a project everything is closed - no window is visible

Show a screenshot where "everything is closed" after opening a project. Is Project Explorer window shown? If not, open it using Window -> Show View -> Project Explorer.

 

> Whe I was very young we had a car

Relevance??

 

> I tried to change dark gray text color background in C/C++ editor and ... surprisingly ...  it is NOT possib

You can change the theme in Window -> Preferences -> General -> Appearance

TDK_0-1739547800946.png

There are more fine grained ways to customize the theme. Search for "eclipse change font color" or similar. However, if you are unable to open a project, it seems like changing the background color should not be a priority.

If you feel a post has answered your question, please click "Accept as Solution".
Imen.D
ST Employee

Hello @JerryMC22 ,

1/ Close STM32CubeIDE completely (End job in Task Manager) and restart it. This might help in refreshing the IDE and resolving any temporary glitches.

2/ This article with detailed steps may help you: How to change STM32CubeIDE to dark theme - STMicroelectronics Community

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

The dark mode in CubeIDE is great idea, but the "gary" text background ? really ?

I would expect black text backgroud.

Really - you have to set it to ...what you like more.

AScha3_0-1739558765848.png

right click -> preferences ...

If you feel a post has answered your question, please click "Accept as Solution".