SysTick does not interrupt in project created by STM32CubeIDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-20 4:58 AM
I used STM3CubeIDE to create a default project (no settings changed) for a stm32l496ve chip. It generates a main file that has:
int main(void)
HAL_Init();
SystemClock_Config();
while (1)
{
}
return 0;
}
And a SysTick_Handler defined in stm32l4xx_it.c:
void SysTick_Handler(void)
{
/* USER CODE BEGIN SysTick_IRQn 0 */
/* USER CODE END SysTick_IRQn 0 */
HAL_IncTick();
/* USER CODE BEGIN SysTick_IRQn 1 */
/* USER CODE END SysTick_IRQn 1 */
}
The startup file startup_stm32l496vetx.s has SysTick defined in the vector table:
_pfnVectors:
.word _estack
.word Reset_Handler
.word NMI_Handler
.word HardFault_Handler
.word MemManage_Handler
.word BusFault_Handler
.word UsageFault_Handler
.word 0
.word 0
.word 0
.word 0
.word SVC_Handler
.word DebugMon_Handler
.word 0
.word PendSV_Handler
.word SysTick_Handler
.word WWDG_IRQHandler
...
...
But despite this, it doesn't seem like the SysTick is being interrupted. HAL_Delay() would cause an infinite loop and a breakpoint at HAL_IncTick in SysTick_Handler() is never called.
Solved! Go to Solution.
- Labels:
-
STM32CubeIDE
-
STM32L4 Series
-
SysTick
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-20 5:07 AM
So I found out why. I moved the start of FLASH to a different address via the linker script. I forgot to change the FLASH_BASE define accordingly in stm32l496xx.h
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-11-20 5:07 AM
So I found out why. I moved the start of FLASH to a different address via the linker script. I forgot to change the FLASH_BASE define accordingly in stm32l496xx.h