cancel
Showing results for 
Search instead for 
Did you mean: 

Internal Errors occurred during the build (1.18.0 on Ubuntu 24.04 LTS)

clement-fr
Visitor

Hello everyone,

I recently installed the application on my computer running Ubuntu 24.04 LTS and created a new project, just like on Windows 10. When I try to build the automatically generated program, I encounter a very confusing error. Here is the error message displayed in the console:

Capture d’écran du 2025-04-04 15-05-50.png

Context:
- STM32CubeIDE version: 1.18.0
- Microcontroller used: STM32G070CBT6
- Project generated with STM32CubeMX
- Operating system: Ubuntu 24.04 LTS

Tests already performed:
- Cleaning and rebuilding the project (Project > Clean... then Build All).
- Resetting the index (Project > C/C++ Index > Rebuild).
- Checking the compiler in Project > Properties > C/C++ Build > Toolchain Editor. Modified the build command (Properties > C/C++ Build > Builder Settings), testing with and without make -j4.
- Re-import the project after deleting the workspace (File > Import > Existing Projects into Workspace).
- Checked the error logs (Window > Show View > Error Log).
- Updated STM32CubeIDE and firmware packs.
- I also tried running the application from a terminal, here is the message: 1 : `Invalid condition id : UX_CORESTACK_Condition cause : null`

Despite these steps, the error persists. Have you encountered this problem before or do you have other avenues to explore?

Thanks in advance for your help!

 

0 REPLIES 0