cancel
Showing results for 
Search instead for 
Did you mean: 

STMCubeIDE Defaults

MikeDB
Lead

In the new project setup, the default minimum heap and minimum stack size are set to 0x200 and 0x400, but despite being in black they seem to be non-editable. For a large processor these numbers are far too small, especially the stack.

And yes I know I can edit the Linker file, as I have done, but really this parameter should be editable on the generation screen, and the default processor range specific. I would suggest stack of at least 0x1000 for a H7 or F7.

3 REPLIES 3
MikeDB
Lead

Bumping this back up in the hope an STM person will reply

Markus GIRDLAND
ST Employee

I can edit those fields and the correct linker script gets generated:

0690X000008iv4YQAQ.png

Is it non-editable for you in every project? I created one for a NUCLEO-H745ZI-Q and STM32H743I-EVAL and they both seem fine.

I did notice that I had to keep the mouse inside the text box in order to edit them, though. Perhaps that is what's causing it?

Ok – yes you need to keep the mouse inside but also turn off Windows screen magnification for those with poor eyesight. It works then and I can then turn magnification back on.
Thanks