2023-12-21 9:19 AM
How do I import the BSP and OSPI_NOR_MemoryMapped examples from the STM32CubeU5 package for the STM32U5A9J-DK board? That series of board is not listed as supported in the example selector, so I have to use the git repo. These are all examples that indicate they were tested with the MB1829B board, which I have.
These examples don't include and IOC file, so that import method doesn't work for these projects.
I tried importing the .project file in the STM32CubeIDE folder. However, that detects it as a nested project and imports everything including the EWARM and MDK-ARM folders and also doesn't import build settings.
What am I doing incorrectly?
2023-12-21 10:13 AM
Unfortunately, you didn't specify how exactly you imported .cproject, but if I click on
File > Import... > General > Existing Project into Workspace > Browse (top right)
to navigate to the project path:
<path>\STM32Cube_FW_U5_V1.xx.0\Projects\STM32U5x9J-DK\Examples\OSPI\OSPI_NOR_MemoryMapped
then STM32CubeIDE only finds and marks one project, namely the one for CubeIDE.
Are you using the most recent version of STM32CubeIDE?
Regards
/Peter
2023-12-21 10:51 AM
I'm using 1.14.0.
I tried this method and then when I try to build, I get multiple errors due to not being able to find "stm32u5xx_hal.h"
I also notice it references other include directories that are empty, such as the hal_driver and cmsis directories. It appears that these are sub repos that git wasn't cloning.
2023-12-21 11:27 AM
I am sorry that I could find nothing helpful. You can raise this issue in github.