STM32L4 series: Bootloader from system memory
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-03 10:22 PM
Hi, I'm using an STM32L4P5ZG microcontroller, trying to do a bootloader program. Entering into bootloader mode, exit after a fraction of a second and jump to the main loop. Not staying in the bootloader mode. I tried enabling through software to PH3 pin as pull-high state as well tried the last option by making nBoot1 =1, nBoot0& nSWBoot0=0. Both returned same, not staying in bootloader mode. Whenever I do manually PH3 boot0 pin as pull-high, entering into bootloader mode.
Code:
HAL_StatusTypeDef SystemBootloaderJump(void)
{
typedef void (*pFunction)(void);
FLASH_OBProgramInitTypeDef OBInit;
uint32_t JumpAddress = SYS_BOOTLOADER_ADDR; // This will be aliased to 0x00000000
pFunction JumpToSystemBoot = (void (*)(void))(JumpAddress);
// Delete the signature bin file
strcat(path, "CFC.bin");
f_unlink (path);
// Alias the system memory from the boot memory space starting @0x1FFF0000
HAL_FLASHEx_OBGetConfig(&OBInit); // OBInit.USERConfig holds OPTR data
OBInit.OptionType = OPTIONBYTE_USER;
OBInit.USERType |= OB_USER_nBOOT1;
OBInit.USERType &= ~(OB_USER_nSWBOOT0 | OB_USER_nBOOT0); // System memory is selected as boot area
// Set new values for the Options page and launch
if (HAL_FLASHEx_OBProgram(&OBInit) == HAL_OK)
{
if (HAL_FLASH_OB_Launch() == HAL_OK)
{
   // Prepare to jump to System Boot Loader
   GPIOH->MODER &= ~(GPIO_MODER_MODE3_1 | GPIO_MODER_MODE3_0); // PH3 as input (BOOT0)
   GPIOH->PUPDR &= ~(GPIO_PUPDR_PUPD3_1 | GPIO_PUPDR_PUPD3_0); // Pull-up enabled for PE3 input
   GPIOH->PUPDR |= GPIO_PUPDR_PUPD3_0;
   GPIOB->MODER &= ~(GPIO_MODER_MODE1_1); // PB1 (Drive_MODE0) as output
   GPIOB->MODER |= GPIO_MODER_MODE1_0;
   HAL_GPIO_WritePin(GPIOB, GPIO_ODR_OD1, GPIO_PIN_SET); // Set PB1 high that drives BOOT0
   //HAL_RCC_DeInit();
   //__disable_irq();
while (1)
{
   Drv_LED(LED_HB, DRV_TOGGLE);
}
SysTick->CTRL = 0;
   SysTick->LOAD = 0;
SysTick->VAL = 0;
//__set_MSP(*(__IO uint32_t*)JumpAddress );
//JumpToSystemBoot = (void (*)(void))(*((uint32_t *)(JumpAddress + 4)));
//__set_MSP(DEF_STACK_STRT_ADDR);
JumpToSystemBoot();
}
}
// Unable to configure the option register / launch the new configuration
return HAL_ERROR;
}
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-04 6:58 AM
Your code is a bit of a mess of commented out statements. It should be clear why it doesn't work in its current state as the __set_MSP line is commented out.
Perhaps take a look at known working code:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-04 6:58 AM
Your code is a bit of a mess of commented out statements. It should be clear why it doesn't work in its current state as the __set_MSP line is commented out.
Perhaps take a look at known working code:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-06 5:03 PM
That code is known to be a broken bloatware as all of the code from the HAL team. The first comment on that article explains and shows it very clearly!