2024-10-01 08:53 AM
Hello
I have created a project for a STM32H745I_Disco board in TouchGFX, imported it to STM32CubeIDE and enabled:
After this, I generated the code. I had to manually add the usb files (STM32_USB_Host_Lib, USB_HOST, FATFS) to the project for it to compile successfully.
Now i want to write to a flash drive connected to the USB_FS port, using the default fatfs functions. All I did in the code is use f_mount, f_open, f_write and f_close for my flash drive, in usb_host.c in USBH_UserProcess under the HOST_USER_CLASS_ACTIVE case, like this:
case HOST_USER_CLASS_ACTIVE:
Appli_state = APPLICATION_READY;
FIL file;
FRESULT res;
char data[] = "Hello, World!";
UINT bytesWritten;
// Attempt to mount the file system
if (f_mount(&USBHFatFS, (TCHAR const*)USBHPath, 0) != FR_OK) {
printf("Mount failed!\n");
return;
}
// Attempt to open the file
printf("Attempting to open the file...\n");
res = f_open(&file, "test.txt", FA_CREATE_ALWAYS | FA_WRITE);
if (res != FR_OK) {
printf("File open failed with error: %d\n", res);
return; // Exit if opening the file fails
}
printf("File opened successfully!\n");
// Attempt to write to the file
printf("Preparing to write data to the file...\n");
res = f_write(&file, data, sizeof(data) - 1, &bytesWritten);
if (res != FR_OK) {
printf("Write operation failed with error: %d\n", res);
} else {
printf("File written successfully! Bytes written: %u\n", bytesWritten);
}
// Attempt to close the file
res = f_close(&file);
if (res != FR_OK) {
printf("File close failed with error: %d\n", res);
} else {
printf("File closed successfully!\n");
}
break;
When debugging, the code is stuck in tasks.c at line 3157: configASSERT( pxUnblockedTCB ); so is it some problem with RTOS scheduling?
When removing parts of my code, f_mount only works fine. Starting from f_open, the code gets stuck.
I have attached my .ioc file, but I really just adjusted the parts mentioned above.
What am I doing wrong here?
2024-10-01 12:39 PM
Hi @FabianEbs
Have you tried this example.
The issue could be linked to the stack/heap size for tasks, you can refer to the config in FreeRTOSConfig.h
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.