User Activity

Hello there :) I create a project with TouchGFX 4.24.1, then import it to CubeIDE 1.16.1, which are both the current versions. Once i open the .ioc file, it says the file need to either be migrated to 6.12.1 or I can use the file as is, which seems t...
Hello :)I have created a project for a STM32H745I_Disco board in TouchGFX, imported it to STM32CubeIDE and enabled:USB_OTG_FS -- Host_Only and VBUS sensingUSB_HOST_M7 -- Mass Storage Host Class + Platform settings for enable PinFATFS_M7 -- USB Disk, ...
I am trying to implement MODBUS-TCP on a TouchGFX generated project. I have successfully enabled Ethernet by following this tutorial on this forum: How to create a project for STM32H7 with Ethernet and LwIP stack working and can ping my board.In the ...
I have tested a TouchGFX-created project that should tie in a USB-Stick connected to the board and create a csv file, then write to it. After writing the necessary code and debugging this project in STM32CubeIDE, the board was stuck with a white scre...
Kudos from
Kudos given to