2020-11-06 3:47 PM
What is ST's response to this document and the fact that I am witnessing such behaviour (see image) ?? Was there simply an error in this document? I was following the doc only to be frustrated by M4 hitting a brick wall with SIGTRAP, there is mention of "option bytes" by user TDK here. Is thee something that I am missing and I can edit these option bytes in either STM32cubeIDE or CUBEMX or is this strictly a CubeProgrammer ability? BOOT_CM4=0 in the option bytes??? Where is this?? Can I change this Via GUI interface?? Should I proceed and think nothing of it and consider this error in document?
Please clarify... Thank you.
https://community.st.com/s/question/0D53W000003MxVD/debugging-stm32h7-dual-core
2020-11-11 11:03 AM
hello