cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer flash works where STM32CubeIDE does'nt

oga
Associate III

I'm not understanding why ( that why I'm here ...cpt obvious speaking) since 2 days I can't flash or debug under CubeIDE while in the same time connection and flash is working perfectly

for the record I'm working on a stm32WB35 using a stlink V3 v

STM32CubeIDE is : 1.15.1

STM32CubeProgrammer is 2.14.0

I've slow down the speed and tried all reset modes

oga_0-1719329457334.png

 

when I'm flashing under CubeIDE I have this results

 

 

 

 

STMicroelectronics ST-LINK GDB server. Version 7.7.0 Copyright (c) 2024, STMicroelectronics. All rights reserved. Starting server with the following options: Persistent Mode : Disabled Logging Level : 1 Listen Port Number : 61234 Status Refresh Delay : 15s Verbose Mode : Disabled SWD Debug : Enabled ST-LINK device status: UNKNOWN Waiting for debugger connection... Debugger connected Waiting for debugger connection... Debugger connected Waiting for debugger connection... ------------------------------------------------------------------- STM32CubeProgrammer v2.16.0 ------------------------------------------------------------------- Log output file: C:\Users\O08A6~1.GAS\AppData\Local\Temp\STM32CubeProgrammer_a17572.log ST-LINK SN : 002C00363331510F34333834 ST-LINK FW : V3J15M6B5S1 Board : STLINK-V3SET Voltage : 2.92V Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication 2nd connect tentative with frequency (8MHz) ST-LINK SN : 002C00363331510F34333834 ST-LINK FW : V3J15M6B5S1 Board : STLINK-V3SET Voltage : 2.92V Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication Encountered Error when opening C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.201.202404072231\tools\bin\STM32_Programmer_CLI.exe Error in STM32CubeProgrammer Shutting down... Exit.
View more

 

 

 

oga_0-1719319822405.png

while under CubeProgrammer I got

 

 

 

14:54:59:978 : UR connection mode is defined with the HWrst reset mode 14:55:00:023 : ST-LINK SN : 002C00363331510F34333834 14:55:00:024 : ST-LINK FW : V3J15M6B5S1 14:55:00:024 : Board : STLINK-V3SET 14:55:00:024 : Voltage : 2.89V 14:55:00:024 : SWD freq : 8000 KHz 14:55:00:024 : Connect mode: Normal 14:55:00:024 : Reset mode : Software reset 14:55:00:024 : Device ID : 0x495 14:55:00:024 : Revision ID : Rev Y 14:55:00:024 : flash loader C:\ST\CubeProgrammer\bin/FlashLoader/0x495.stldr is loaded 14:55:00:024 : Debug in Low Power mode enabled. 14:55:00:275 : UPLOADING OPTION BYTES DATA ... 14:55:00:275 : Bank : 0x00 14:55:00:275 : Address : 0x58004020 14:55:00:275 : Size : 96 Bytes 14:55:00:277 : Bank : 0x01 14:55:00:277 : Address : 0x58004080 14:55:00:277 : Size : 8 Bytes 14:55:00:277 : UPLOADING OPTION BYTES DATA ... 14:55:00:277 : Bank : 0x00 14:55:00:277 : Address : 0x58004020 14:55:00:277 : Size : 96 Bytes 14:55:00:278 : Bank : 0x01 14:55:00:278 : Address : 0x58004080 14:55:00:278 : Size : 8 Bytes 14:55:00:278 : UPLOADING ... 14:55:00:278 : Size : 4 Bytes 14:55:00:278 : Address : 0x58004080 14:55:00:278 : Read progress: 14:55:00:279 : Data read successfully 14:55:00:279 : Time elapsed during the read operation is: 00:00:00.001 14:55:00:279 : UPLOADING ... 14:55:00:279 : Size : 1024 Bytes 14:55:00:279 : Address : 0x8000000 14:55:00:279 : Read progress: 14:55:00:280 : Data read successfully 14:55:00:280 : Time elapsed during the read operation is: 00:00:00.003 14:55:02:848 : Memory Programming ... 14:55:02:848 : Opening and parsing file: RS_Mk3.hex 14:55:02:854 : File : RS_Mk3.hex 14:55:02:854 : Size : 104.42 KB 14:55:02:854 : Address : 0x08000000 14:55:02:854 : Erasing memory corresponding to segment 0: 14:55:02:855 : Memory Erase via FlashLoader! 14:55:02:855 : Memory erase... 14:55:02:860 : halt ap 0 14:55:02:865 : Erasing internal memory sectors [0 26] 14:55:02:866 : Init flashloader... 14:55:02:866 : halt ap 0 14:55:02:868 : run ap 0 14:55:02:868 : halt ap 0 14:55:02:868 : Loader sector erase... 14:55:02:874 : run ap 0 14:55:03:468 : halt ap 0 14:55:03:468 : Download in Progress: 14:55:03:469 : Size : 106936 Bytes 14:55:03:469 : Address : 0x08000000 14:55:03:471 : halt ap 0 14:55:03:478 : Loader write range... 14:55:03:587 : Init flashloader... 14:55:03:587 : halt ap 0 14:55:03:592 : run ap 0 14:55:03:593 : halt ap 0 14:55:03:598 : run ap 0 14:55:04:316 : run ap 0 14:55:05:030 : Segment[0] downloaded successfully 14:55:05:030 : File download complete 14:55:05:047 : Time elapsed during download operation: 00:00:02.179 14:55:05:047 : Verifying ... 14:55:05:047 : Read progress: 14:55:05:303 : Download verified successfully 14:55:05:326 : RUNNING Program ... 14:55:05:326 : Address: : 0x08000000 14:55:05:327 : Application is running, Please Hold on... 14:55:05:327 : Start operation achieved successfully
View more

 

 

 

unfortunately the log file is not found in the named folder

I feel lost any help would be greatly appreciated

thanks a lot bu advance

 

0 REPLIES 0