cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE v1.15 Wrapping read detected

ABouk.1
Associate III

Hello,

 

I am experiencing a bug in STM32CubeIDE since I made the latest update 2 days ago.

I was able to download the SW and debug in the previous version, after the updage I can't even download the software using STM32CubeID here is the log :

STMicroelectronics ST-LINK GDB server. Version 7.8.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Wrapping read detected. Addr: 0xffffffff; Length: 8

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 8

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 8

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 8

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 8

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 8

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 8

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 8

Wrapping read detected. Addr: 0xffffffff; Length: 1

Wrapping read detected. Addr: 0xffffffff; Length: 1

Debugger connected

Waiting for debugger connection...

xShutting down...

Exit.

3 REPLIES 3
ABouk.1
Associate III

I have downloaded the latest STM32CubeIDE version (1.16) and set the debug configuration (ST-LINK GDB). Now, starting a debug session doesn't erase the flash/load the program and jumps directly to the program already existing in the FLASH memory. I have checked the "download" checkbox in the startup tab

ABouk.1
Associate III

Capture d’écran 2024-07-05 113157.pngCapture d’écran 2024-07-05 113059.pngCapture d’écran 2024-07-05 113215.png

 

gyurma888
Associate

Hi, 

I have the same problem as you. Do you know what is the solution to this error? 

I updated the program just now from 1.14 to 1.17.