cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE TIM15 OPM settings are missing

PKurz.1
Associate III

Hi,

STM32CubeIDE Version: 1.14.1 (and earlier)

PKurz1_0-1709506014067.png

after selecting One Pulse Mode, the settings for this operating mode do not appear.

 
 
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @PKurz.1 ,

 

Thank you for bringing this issue to our attention.

An internal ticket is submitted to the development team (Internal Ticket Number: 216008).

I will keep you up to date when the issue is solved.

 

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

11 REPLIES 11
TDK
Super User

What settings do you think should be there? Did you perhaps mean to set it to PWM generation instead of output compare? What chip?

 

If you feel a post has answered your question, please click "Accept as Solution".
PKurz.1
Associate III

Sorry for the inaccuracy, what I mean is that the Retriggerable OPM mode 1/2 option is missing.

I use STM32F303.

 

It's been over a year and it's still missing...

Hello @PKurz.1 ,

 

Let me thank you for posting.

Your request is under investigation, and I will get back to you as soon as possible.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @PKurz.1 ,

 

Thank you for bringing this issue to our attention.

An internal ticket is submitted to the development team (Internal Ticket Number: 216008).

I will keep you up to date when the issue is solved.

 

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Is there an estimated completion time?

 

regards

PKurz.1
Associate III

How many years do you have to wait?

 

regards

cyber_v1
Associate III

+ TIM16 and TIM17 doesn't seem to have the setting for the One Pulse Mode at all. They're always configured in OPM.

PKurz.1
Associate III

It will soon be 2 years since the report was filed 

regards