2023-08-24 8:39 AM - edited 2023-08-24 8:54 AM
yesterday installed new ide 13.1 , because H563-nucleo board not working with "old" v10.
after some trouble with new "forced login feature" i could make new project from H563 examples.
then i could compile and flash / debug. seem ok so far, then close and shutdown.
then today, start IDE ( on this new workspace) and it cannot start - just "an error has occurred. see log file...metadata.log" .
come on, what now?
i seen a comment, if problem with new v13 , just delete metadata (ok, i moved to other directoty, to be able to use it again.)
then ide starting up, bt no projects found. ok, i "open new..from filesystem" and it is here again.
but now...cannot compile ! -> error " warning: no encoding set .." . hmmm...
close ide.
open again...and voila : "an error has occurred. see log file...metadata.log" .
perfect.
what can i do now ???
2023-08-25 12:33 AM
Hello AScha.3.
First I would like to thank you for your feedback, it helps us to constantly improve our products.
To help to dig into your symptoms analysis, is that possible that you share the content of the log files.
In your workspaces directories, there is a directory name .metadata.
Could you please make a zip of all files that are located in this .metadata folder (do not include the subdirectories).
Great thanks in advance.
2023-08-25 12:52 AM
Hello @Sirma Siang ,
here the log of the v13.1 install...made 1 project, compile, debug...ok. close.
open ide next day....error. no work.
btw. zip upload not allowed here !!!!! (what a pita...) made rar file.
2023-08-25 10:55 AM
:see_no_evil_monkey:
2023-08-28 2:01 PM - edited 2023-08-29 5:02 AM
Hi, @Sirma Siang ,
you seen my ...log ?
any idea about ?
btw i tried re-install, make new project - works. next start same : error, see log. no chance to work with STM32IDE.
2023-08-28 3:06 PM
> warning: no encoding set
Try this: in a new workspace, before importing 1st project: open Window-> Preferences->Workspace
Check that Text file encoding is selected (recommended UTF-8).
2023-08-29 4:45 AM
thx @Pavel A. ,
i tried open new workspace - Text encoding is set to UTF-8 . seem ok. so close IDE, without any project now.
IDE open/start in this empty workspace ok. (great achievement :) ) .
then import (-from existing project) . -> build/compile greyed out, cannot compile. (dont know why...no message.)
ok ok, new project, stm -> from cpu selection, choose F303cbt6. Oooo - cannot download mx..., need to login ti my.st , very great idea, this move. makes me feel very good about STM .
closing actual window, can generate code now. wow. then download 150MB ...can compile now.
now the TEST : close and open ide then... dazong. no more ide , error -> see log file.
i think, i give up on this....
any tips, what i should try now ? VScode with stm extension?
2023-09-01 5:20 AM
today new idea: on my PC is also a almost unused Win10/64 partition, so i start this "virgin" Win10 and installed new IDE 13.1.
first test project: new F303 stm32 project, cube-gen.code-compile all ok. close ide, open again - seem ok.
then new H563 project, with Azure RTOS + USB audio host , cube-gen.code-compile -> 1 error , a header file missing.
close IDE , open --- error (again same) -> see log file.
so seems impossible to work with H563 on IDE 13.1 on Win10.
can open ide and make new project, compile and debug - but only until ide is closed. never start again.
any help on this misery ?
2023-09-03 12:03 AM - edited 2023-09-03 12:04 AM
--- and with new, empty workspace is starting, can make new projects etc, until closing IDE . never open again.
except on new, empty workspace.
Hello @mattias norlander ,
Can you please help on this issue related to CubeIDE?