cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE: Is it possible to flash without debugging the old STM32VLDiscovery directly from the software? When using the debug or run button I get "Debug not supported".

evenlund
Associate III
 
4 REPLIES 4
TDK
Guru

The latest release added the capability to run without debugging.

If you feel a post has answered your question, please click "Accept as Solution".
evenlund
Associate III

I think I already have the latest version. What do I change to run without debugging?

Ozone
Lead III

I think this boils down to "is the obsolete ST-Link V1 supported by STM32CubeIDE ?".

evenlund
Associate III

The discovery board is at least available in STM32CubeIDE. Is there a way to flash the firmware generated by the CubeIDE in a different software then?