2020-02-21 08:10 AM
Hi,
I wanted to start learning FreeRTOS. I'm working with a L082 device, using CubeIDE. In the config file, I only can select CMSIS-RTOS v1 interface, v2 is disabled. But there's no explanation why.
So, I don't know if the device is unsupported by v2 or if there's something missing. I assume I can get it to work with v1, but...
Regards
Solved! Go to Solution.
2020-02-23 07:53 AM
> So, I don't know if the device is unsupported by v2 or if there's something missing. I assume I can get it to work with v1, but...
When you hoover the mouse over CMSIS_V2 is lists the supported series. L0 is not among them.
2020-02-23 07:53 AM
> So, I don't know if the device is unsupported by v2 or if there's something missing. I assume I can get it to work with v1, but...
When you hoover the mouse over CMSIS_V2 is lists the supported series. L0 is not among them.
2020-02-23 10:51 PM
Ah, okay. Thank you. Sometimes it's not clear if an option is disabled because of missing settings or because the device doesn't support it. Now it's clear.
Regards