cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE build problem on closed server in company via TCP/IP

HYILD.2
Associate

Hello, After creating a project on the SSD in the computer, I have no problems compiling this project. But I cannot compile the project (over TCP/IP) that I created in the server in the company. I keep getting the error "No such file or directory" when I try to compile. What is the reason of this?

(Example file path where I am trying to build and compile the project: \\10.0.0.4\bnz-fs\AKN02\AKN02-1A\BNZ02-1B-304\ELECTRONICS\SOFTWARE\MyExamplePROJECT )

1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Evangelist III

Can you ask your IT person to help? They probably would advise mapping a drive letter to your server (net use N:  \\10.0.0.4\bnz-fs .... )

View solution in original post

2 REPLIES 2
Pavel A.
Evangelist III

Can you ask your IT person to help? They probably would advise mapping a drive letter to your server (net use N:  \\10.0.0.4\bnz-fs .... )

Thanks Pavel, After mapping the server to a drive letter, the issue was resolved.