2022-08-16 03:15 AM
Hello,
Two questions.
First one: __attribute__((__packed__)) does not work: for a structure
typedef __attribute__((__packed__)) struct a_s {
uint32_t M;
uint16_t V;
uint8_t Data[1];
} Type_A;
sizeof(Type_A) returns 8, not 7.
Second one: after STM32CubeIDE update to 1.10.1 when "Build a selected file" (*.c), the file seems to be processed, but NO build results more seen in the CDT Build Console.
Any ideas?
Solved! Go to Solution.
2022-08-24 02:45 AM
Thanks for your replies.
2022-08-24 05:27 AM
Thanks! I inserted
static_assert(sizeof(Type_A) == 7);
for the case in my code...
2022-08-24 07:01 AM
To the second question about "no console output while building a single file".
I found out, that in the "good" workspace I can choose either "internal" or "external" builder under "Properties->C/C++ Build->Builder Settings", and both work fine. Besides, if I build a single file, regardless of the setting, the console shows:
15:59:45 **** Building Selected Files of configuration Debug for project CAT ****
Info: Internal Builder is used for build
...
15:59:45 Build Finished. 0 errors, 0 warnings. (took 301ms)
In the "bad" workspace choosing the "internal" builder and trying to build a project, a severe error occures:
Errors occurred during the build.
Errors running builder 'CDT Builder' on project 'Basic'.
Internal error building project Basic configuration Debug
java.lang.NullPointerException
Internal error building project Basic configuration Debug
java.lang.NullPointerException
So, I think, the problem is not in the console but in the fact, that the internal builder is invoked to build a single file, it crashes, and the console has nothing to show!
Now the question is, how to repare this issue with the internal builder?
2022-08-24 08:20 AM
About the second question I think that you accidently clicked on "Pin Console".
Check if the button shown in the screenshot is not pressed on any console in your workspace.
Kind regards,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-24 08:42 AM
In the "good" workspace it does not matter, pinned or not: I see the output of the builder anyway. The main issue is no more the console but the fact, under the "bad" workspace the internal builder crashes:
Later, since for building of a single file always the internal builder seems to be engaged, it crashes silently, and the console shows nothing...
2022-08-25 02:16 AM
Hello @ColdWeather
Could you please send me the workspace .log file to be able to further do analysis the issue.
This file is found under the workspace directory under ".metadata".
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-25 02:28 AM
Thank you for helping me!
I discovered an interesting thing: under the "bad" workspace I have actually two projects: "Basic" and "Mowitec", and the last one can be switched to the internal builder w/o any issue! Thus, it must be some project setting(s) for "Basic" that make(s) the internal builder crash.
I closed the IDE, deleted *.log files, started again and built both "Mowitec" and "Basic". The log file is under the link:
https://drive.google.com/file/d/1WevKLwnb2cl6cEYKfyFCk7fLMwwM7zX2/view?usp=sharing
2022-08-27 07:42 AM
Another ST employee not even understanding the problem (structure packing) because of a lack of the basic C language and compiler knowledge...
2022-08-29 01:13 AM
Hello
We do not support the CDT internal builder.
May I ask why you want to use the Internal builder?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-30 11:10 PM
I'm afraid, you did not read my previous report regarding two projects under the workspace with the issue. Regardless of your assert, if you support or not the internal builder, the symptoms are that the IDE does support both builders, and when building/translating a single file the internal builder is engaged regardless of the project setting "use internal" or ".. external" builder. I have no issue to use the external one (and I do it!), but the point is, I cannot build a single file (what I used to as a convenient way to check the syntax quickly) because the IDE seems to engage always the internal one for this purpose that crashes in my project "Basic". At the same time, in the same workspace(!), another similar project generates no errors when building a single file. Conclusions: