2021-02-24 07:00 AM
STM32CubeIDE 1.6.0 was released this week on st.com as well as a in-tool update patch.
Caution: The in-tool update does not allow updating drivers and ST-LINK server tool. Full installer is required for this.
What is new in 1.6.0? (only some highlights)
Main issues fixed in STM32CubeIDE 1.6.0
Only a sub-set of the many tickets closed are mentioned in the release note.
Known problems and limitations
Please refer to the release note.
Where do I Obtain CubeIDE 1.6.0?
2021-03-04 07:05 AM
The thread is growing... It is becoming hard to follow the discussion both for support-team and end-users.
Feel free to reply to already identified issues in this thread.
But - please submit any new issue/feedback in new threads. Thanks!
2021-03-27 08:45 PM
Hi,
I am also facing the same issue, any resolution for the same.Regards
Sai Ram Mannar
2021-05-05 05:52 AM
When you say "Play" what is the fix. Shouldn't it work by default on the nucleo board and which bit needs correcting as its now broken.
I'm happy to "play" but really we should know the exact correction as it could affect other things.
Thanks,
Mark