2020-11-23 02:59 AM
Hi,
I cannot import existing project into Workspace. Here's the error log when I try to select a root directory:
eclipse.buildId=Version 1.5.0
java.version=1.8.0_272
java.vendor=AdoptOpenJDK
BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_US
Command-line arguments: -os linux -ws gtk -arch x86_64
org.eclipse.ui.workbench
Error
Mon Nov 23 11:08:37 CET 2020
Unhandled event loop exception
org.eclipse.swt.SWTError: No more handles
at org.eclipse.swt.SWT.error(SWT.java:4749)
at org.eclipse.swt.SWT.error(SWT.java:4638)
at org.eclipse.swt.SWT.error(SWT.java:4609)
at org.eclipse.swt.widgets.Dialog.error(Dialog.java:202)
at org.eclipse.swt.widgets.DirectoryDialog.openNativeChooserDialog(DirectoryDialog.java:139)
at org.eclipse.swt.widgets.DirectoryDialog.open(DirectoryDialog.java:123)
at org.eclipse.ui.internal.wizards.datatransfer.WizardProjectsImportPage.handleLocationDirectoryButtonPressed(WizardProjectsImportPage.java:1209)
at org.eclipse.ui.internal.wizards.datatransfer.WizardProjectsImportPage$7.widgetSelected(WizardProjectsImportPage.java:726)
at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:252)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5685)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1423)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4953)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:4446)
at org.eclipse.jface.window.Window.runEventLoop(Window.java:823)
at org.eclipse.jface.window.Window.open(Window.java:799)
at org.eclipse.ui.internal.handlers.WizardHandler$Import.executeHandler(WizardHandler.java:151)
at org.eclipse.ui.internal.handlers.WizardHandler.execute(WizardHandler.java:280)
at org.eclipse.ui.internal.handlers.HandlerProxy.execute(HandlerProxy.java:283)
at org.eclipse.ui.internal.handlers.E4HandlerProxy.execute(E4HandlerProxy.java:97)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:58)
at org.eclipse.e4.core.internal.di.InjectorImpl.invokeUsingClass(InjectorImpl.java:319)
at org.eclipse.e4.core.internal.di.InjectorImpl.invoke(InjectorImpl.java:253)
at org.eclipse.e4.core.contexts.ContextInjectionFactory.invoke(ContextInjectionFactory.java:173)
at org.eclipse.e4.core.commands.internal.HandlerServiceHandler.execute(HandlerServiceHandler.java:156)
at org.eclipse.core.commands.Command.executeWithChecks(Command.java:488)
at org.eclipse.core.commands.ParameterizedCommand.executeWithChecks(ParameterizedCommand.java:487)
at org.eclipse.e4.core.commands.internal.HandlerServiceImpl.executeHandler(HandlerServiceImpl.java:213)
at org.eclipse.ui.internal.handlers.LegacyHandlerService.executeCommand(LegacyHandlerService.java:389)
at org.eclipse.ui.internal.handlers.LegacyHandlerService.executeCommand(LegacyHandlerService.java:366)
at org.eclipse.ui.internal.views.helpers.EmptyWorkspaceHelper$ImportAction.run(EmptyWorkspaceHelper.java:393)
at org.eclipse.ui.internal.views.helpers.EmptyWorkspaceHelper$1.linkActivated(EmptyWorkspaceHelper.java:275)
at org.eclipse.ui.forms.widgets.AbstractHyperlink.handleActivate(AbstractHyperlink.java:215)
at org.eclipse.ui.forms.widgets.AbstractHyperlink.handleMouseUp(AbstractHyperlink.java:309)
at org.eclipse.ui.forms.widgets.AbstractHyperlink.lambda$3(AbstractHyperlink.java:117)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5685)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1423)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4953)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:4446)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1158)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1047)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:658)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:557)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:154)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:150)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:137)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:107)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:657)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:594)
at org.eclipse.equinox.launcher.Main.run(Main.java:1447)
at org.eclipse.equinox.launcher.Main.main(Main.java:1420)
Any hints?
gaston
Solved! Go to Solution.
2020-12-01 02:06 AM
Hello Gaston,
I've ran some import tests on the Linux distributions that we support, Ubuntu® LTS 18.04, LTS 20.04, Fedora® 29 and Fedora® 31. However, I wasn't able to reproduce the problem so my guess is that it might be something specific to Mint but I don't have a test environment for that distribution since we don't officially support it.
Do you have another OS you could try the use case on and see if you face the same issue?
2020-11-23 03:56 AM
Is this for any directory you choose or a specific one?
What version of Linux are you using?
2020-11-23 04:06 AM
Is this for any directory. Just after clicking the "Browse..." buttom
I've used the previous version 1.4.0 with no problems on my Linux Mint 18.3 64-bit
gaston
2020-11-23 05:10 AM
I'll see if I can set up a test environment to reproduce the problem and I'll get back to you with my findings.
2020-11-26 04:26 AM
Hi Markus,
Do you have any news about this problem? I still can't import an existing project.
gaston
2020-12-01 02:06 AM
Hello Gaston,
I've ran some import tests on the Linux distributions that we support, Ubuntu® LTS 18.04, LTS 20.04, Fedora® 29 and Fedora® 31. However, I wasn't able to reproduce the problem so my guess is that it might be something specific to Mint but I don't have a test environment for that distribution since we don't officially support it.
Do you have another OS you could try the use case on and see if you face the same issue?
2020-12-01 07:40 AM
Hi Markus,
I've finally update my GTK+ version from v3.18 to v3.20. Now it works as expected.
Thank you for all anyway,
gaston