2023-10-23 03:06 PM - edited 2023-10-23 03:08 PM
I installed STM32CubeIDE 1.13.2 in the hope that the problem of the 1.13.1 release has been solved (see My old topic ) . Nothing the problem continues to exist. To make the integrated CubeMX work I have to open and close the IDE 3 or 4 times, also if it doesn't start I have to delete the home/user/workspace_1.13.2/.metadata directory. (for my system config see My old topic )
Thanks for your help.
Ferdinando
Solved! Go to Solution.
2024-04-29 01:11 PM
Hi!
Are there any news.
I installed the debian package Stm32CubeIDE 1.15.0 but the problem remained the same if not worse.
I tried to install the Linux Generic 1.15.1 version and modified the stmcudeide_wayland file, with sudo privileges, by adding the line "export GTK_THEME=Adwaita" after the line "export GDK_BACKEND=x11".
Now it work at 95%, occasionally it still crashes, but just close and relaunch the program.
You no longer need to delete any files.
However, I hope for further improvement.