cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.13.0 MPU config causes hard faults

Yaroslav Vushnevsky
Associate II

Hello. I have a project which was worked fine about 3 years. But after update to 1.13.0 I am catching a hard faults at start. I am discover that hard fault happens inside MPU_Config(); function. Also I found that new version has change init order:

YaroslavVushnevsky_0-1689767133402.png

And here is my  MPU_Config:

 

 

void MPU_Config(void)
{
  MPU_Region_InitTypeDef MPU_InitStruct = {0};

  /* Disables the MPU */
  HAL_MPU_Disable();

  /** Initializes and configures the Region and the memory to be protected
  */
  MPU_InitStruct.Enable = MPU_REGION_ENABLE;
  MPU_InitStruct.Number = MPU_REGION_NUMBER0;
  MPU_InitStruct.BaseAddress = 0x30040000;
  MPU_InitStruct.Size = MPU_REGION_SIZE_256B;
  MPU_InitStruct.SubRegionDisable = 0x0;
  MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
  MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
  MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
  MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
  MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
  MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;

  HAL_MPU_ConfigRegion(&MPU_InitStruct);

  /** Initializes and configures the Region and the memory to be protected
  */
  MPU_InitStruct.Number = MPU_REGION_NUMBER1;
  MPU_InitStruct.BaseAddress = 0x30044000;
  MPU_InitStruct.Size = MPU_REGION_SIZE_16KB;
  MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
  MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
  MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

  HAL_MPU_ConfigRegion(&MPU_InitStruct);

  /** Initializes and configures the Region and the memory to be protected
  */
  MPU_InitStruct.Number = MPU_REGION_NUMBER2;
  MPU_InitStruct.BaseAddress = 0x24000000;
  MPU_InitStruct.Size = MPU_REGION_SIZE_512KB;

  HAL_MPU_ConfigRegion(&MPU_InitStruct);

  /** Initializes and configures the Region and the memory to be protected
  */
  MPU_InitStruct.Number = MPU_REGION_NUMBER4;
  MPU_InitStruct.BaseAddress = 0x08100000;
  MPU_InitStruct.Size = MPU_REGION_SIZE_1MB;
  MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;

  HAL_MPU_ConfigRegion(&MPU_InitStruct);
  /* Enables the MPU */
  HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

 

 

Can someone point me what is wrong? Is it IDE bug or my mistake?

P.S. It is H743IIT MCU

P.P.S My fix is to add my own MPU_Config(); call in the user section at begin of main(). Now second call generated with CubeMX will not crash program and CubeMX project update will not delete my fix. I think it is temporary solution and hope will be some fix in next Cube Ide version. 

1 REPLY 1
CMYL
ST Employee

Hi @Yaroslav Vushnevsky 

There is nothing wrong in the MPU configuration.

Did you changed the order of calling caches enable and MPU according to the old scheme ?

If you enable D-cache and then configure your data memory (stack or RW data) to be non-cacheable
(similar to the MPU configuration in new as shown by figure above), some issues may occur.
In such cases, we recommend cleaning the D-cache just before enabling the MPU.

 

Best regards