cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 with simcom A7672S

sreedharan1196
Associate II
#include "main.h"
 
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
 
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#define GETCHAR_PROTOTYPE int __io_getchar(void)
 
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart2;
 
PUTCHAR_PROTOTYPE
{
    HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
    return ch;
}
 
GETCHAR_PROTOTYPE
{
    uint8_t ch = 0;
    __HAL_UART_CLEAR_OREFLAG(&huart2);
    HAL_UART_Receive(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
    return ch;
}
 
int id = 212200;
 
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USART2_UART_Init(void);
 
void parseCmd(char* command, int timeout);
 
int main(void)
{
  setvbuf(stdin, NULL, _IONBF, 0);
 
  HAL_Init();
 
  SystemClock_Config();
 
  MX_GPIO_Init();
  MX_USART1_UART_Init();
  MX_USART2_UART_Init();
 
  HAL_GPIO_WritePin(Enable_key_GPIO_Port, Enable_key_Pin, GPIO_PIN_SET);
  HAL_Delay(2000);
  HAL_GPIO_WritePin(Power_key_GPIO_Port, Power_key_Pin, GPIO_PIN_RESET);
  HAL_Delay(2000);
 
  printf("Sending AT commands...\n");
 
  while (1)
  {
  char strAT[50];
  parseCmd("AT\r\n", 1000); //Check AT
  parseCmd("ATE1\r\n", 1000);
  parseCmd("AT+CSQ\r\n", 1000);
  parseCmd("AT+CPIN?\r\n", 1000);
  parseCmd("AT+CREG=1\r\n", 1000);
  parseCmd("AT+CGREG?\r\n", 1000);
  parseCmd("AT+CGATT=1\r\n", 1000);
  parseCmd("AT+QIFGCNT=0\r\n", 1000);
  parseCmd("AT+QICSGP=1,\"WWW\",\"\",\"\"\r\n", 1000);
  parseCmd("AT+QIREGAPP\r\n", 1000);
  parseCmd("AT+QIACT\r\n", 1000);
  HAL_Delay(2000);
  sprintf(strAT, "AT+QHTTPURL=%d,%d", str_len, 180);
  //Serial.println(strAT);
  printf("The string %s",strAT);
  parseCmd(strAT, 1000);
  parseCmd(json_1, 3000);
  parseCmd("AT+QHTTPPOST=60", 3000);
  parseCmd("AT+QHTTPREAD", 3000);
  parseCmd("AT+QIDEACT", 1000);
 
void parseCmd(char* command, int timeout)
{
    HAL_Delay(timeout);
    char rxdata[300];
    memset(rxdata, 0, sizeof(rxdata));
    // Transmit command over UART1
    HAL_UART_Transmit(&huart1, (uint8_t*)command, strlen(command), timeout);
    // Receive response over UART1
    HAL_UART_Receive(&huart1, (uint8_t *)rxdata, sizeof(rxdata), timeout);
    // Transmit response over UART2
    HAL_UART_Transmit(&huart2, (uint8_t *)rxdata, strlen((char *)rxdata), timeout);
}
 
OUTPUT:
10:29:51.329 -> AT
10:29:51.329 -> OK
10:29:53.295 -> ATE1
10:29:53.295 -> OK
10:29:54.323 -> AT
 
i am using the above AT commands in simcom A7672S ,i am unable to get the proper response from the simcom, may, i know what the issues i am facing, Guide me with the issues i am facing her and help me to sort out this issues
21 REPLIES 21
Techn
Senior II

Firstly chek if the module is able to receive call from another mobile. JUST call that number and check ring back tone. Connect the module to computer using a USB to ttl converter and chek if the module behaves properly.  ATD your number to initiate a  call from mobile.  AT+CSQ for signal strength etc..

 

sreedharan1196
Associate II

thanks for the response, i clear that issues, now i am facing an issue with response received, i am able to get only the half the  response code from the simcom, what tha issues with the above code, help me to short out it

 

char ATcommand[200];

void parseCmd(char *command, int http_time)
{
char rxdata1[1000];
memset(rxdata1, 0, sizeof(rxdata1));

// printf("The AT : %s\r\n",command);

// Transmit command over UART1
HAL_UART_Transmit(&huart1, (uint8_t*)command, strlen(command),http_time);

// Receive response over UART1
HAL_UART_Receive(&huart1, (uint8_t *)rxdata1, sizeof(rxdata1),http_time);

// Transmit response over UART2
HAL_UART_Transmit(&huart2, (uint8_t *)rxdata1, strlen(rxdata1),100);

}

sprintf(ATcommand,"AT+HTTPPARA=\"URL\",\"http://iot.salieabs.in:5003/api/postDeviceDatadev=2122001&mr=108&warn=Done\"\r\n");
parseCmd(ATcommand,2000);

 

output:

11:21:33.298 -> ceData?dev=2122001&mr=108&warn=Done"
11:21:33.298 -> OK

 

verify with it, its working properly, for sms, and Call, also for all other AT commands, but the only issues is 

sprintf(ATcommand,"AT+HTTPPARA=\"URL\",\"http://iot.salieabs.in:5003/api/postDeviceDatadev=2122001&mr=108&warn=Done\"\r\n");

 

for the above AT commands i am getting only the below response, the response is ok thats not the issues, issue is for User interface i am not getting the full response 

 

output:

11:21:33.298 -> ceData?dev=2122001&mr=108&warn=Done"
11:21:33.298 -> OK

 

 

Looks like you have enabled local echo, other wise I guess the response will be "OK", what is the expected output?

 

Andrew Neil
Evangelist III

On debugging serial comms:

https://www.avrfreaks.net/s/topic/a5C3l000000UaFXEA0/t153137?comment=P-1212903 

 

Please use this button to properly post source code:

AndrewNeil_0-1716454761104.png

 

#DebugSerialComms

 

CURRENT OUTPUT :

11:21:33.298 -> ceData?dev=2122001&mr=108&warn=Done"
11:21:33.230 -> OK

 

EXPECTED OUTPUT :

11:21:33.298 -> http://iot.salieabs.in:5003/api/postDeviceData?dev=2122001&mr=108&warn=Done
11:21:33.230 -> OK

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2024 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
const char apn[]  = "WWW";
char ATcommand[200];

char Warning_status[] = "Done";
char Count[] = "10";
char devID[] = "2122001";

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#define GETCHAR_PROTOTYPE int __io_getchar(void)

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */
PUTCHAR_PROTOTYPE
{
    HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
    return ch;
}
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

void  parseCmd(char *command, int delay)
{
	// HAL_UART_Init(&huart1);

	 char rxdata[100];
	 memset(rxdata, 0, sizeof(rxdata));
	 HAL_UART_Transmit(&huart1,(uint8_t*)command,strlen(command),delay);
     HAL_UART_Receive(&huart1,rxdata,sizeof(rxdata),delay);
     HAL_UART_Transmit(&huart2,rxdata,sizeof(rxdata),1000);

     //HAL_UART_DeInit(&huart1);
}

void ExecuteHTTPGetRequest()
{
	 parseCmd("AT\r\n",2000);
	 parseCmd("AT+CSQ\r\n",2000);
	 parseCmd("AT+CREG?\r\n",2000);
	 parseCmd("AT+CGREG?\r\n",5000);
	 parseCmd("AT+CEREG=1\r\n",5000);
	 parseCmd("AT+CPSI?\r\n",2000);
	 parseCmd("AT+CGACT=1,1\r\n",10000);
	 parseCmd("AT+CGATT=1\r\n",2000);
	 parseCmd("AT+CGREG?\r\n",2000);
	 sprintf(ATcommand,"AT+CGDCONT=1,\"IP\",\"%s\"\r\n",apn);
	 parseCmd(ATcommand,4000);
	 parseCmd("AT+HTTPINIT\r\n", 12000);
	 parseCmd("AT+HTTPPARA=\"URL\",\"http://iot.salieabs.in:5003/api/postDeviceData?dev=2122001&mr=108&warn=Done\"\r\n",12000);
	 parseCmd("AT+HTTPACTION=1\r\n",10000);
	 parseCmd("AT+HTTPTERM\r\n",5000);
}
/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART1_UART_Init();
  MX_USART2_UART_Init();
  /* USER CODE BEGIN 2 */
  HAL_GPIO_WritePin(Enable_key_GPIO_Port, Enable_key_Pin, GPIO_PIN_SET);
  HAL_Delay(2000);
  HAL_GPIO_WritePin(Power_key_GPIO_Port, Power_key_Pin, GPIO_PIN_RESET);
  HAL_Delay(2000);

  printf("Initializing HTTP connection...\n");

  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
	  ExecuteHTTPGetRequest();
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

  /** Configure the main internal regulator output voltage
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
  RCC_OscInitStruct.MSIState = RCC_MSI_ON;
  RCC_OscInitStruct.MSICalibrationValue = 0;
  RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
  {
    Error_Handler();
  }
  PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART2;
  PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
  PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief USART1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_USART1_UART_Init(void)
{

  /* USER CODE BEGIN USART1_Init 0 */

  /* USER CODE END USART1_Init 0 */

  /* USER CODE BEGIN USART1_Init 1 */

  /* USER CODE END USART1_Init 1 */
  huart1.Instance = USART1;
  huart1.Init.BaudRate = 115200;
  huart1.Init.WordLength = UART_WORDLENGTH_8B;
  huart1.Init.StopBits = UART_STOPBITS_1;
  huart1.Init.Parity = UART_PARITY_NONE;
  huart1.Init.Mode = UART_MODE_TX_RX;
  huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart1.Init.OverSampling = UART_OVERSAMPLING_16;
  huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_RXOVERRUNDISABLE_INIT;
  huart1.AdvancedInit.OverrunDisable = UART_ADVFEATURE_OVERRUN_DISABLE;
  if (HAL_UART_Init(&huart1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART1_Init 2 */

  /* USER CODE END USART1_Init 2 */

}

/**
  * @brief USART2 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_USART2_UART_Init(void)
{

  /* USER CODE BEGIN USART2_Init 0 */

  /* USER CODE END USART2_Init 0 */

  /* USER CODE BEGIN USART2_Init 1 */

  /* USER CODE END USART2_Init 1 */
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 115200;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART2_Init 2 */

  /* USER CODE END USART2_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(Enable_key_GPIO_Port, Enable_key_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(Power_key_GPIO_Port, Power_key_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pin : Enable_key_Pin */
  GPIO_InitStruct.Pin = Enable_key_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(Enable_key_GPIO_Port, &GPIO_InitStruct);

  /*Configure GPIO pin : Power_key_Pin */
  GPIO_InitStruct.Pin = Power_key_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(Power_key_GPIO_Port, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Andrew Neil
Evangelist III

@sreedharan1196 wrote:
 
  parseCmd("AT\r\n", 1000); //Check AT

Note that the standard AT command terminator is just CR - not CRLF.

 


@sreedharan1196 wrote:
10:29:53.295 -> ATE1
10:29:53.295 -> OK

Why are you turning Echo on?

This means that the modem will send back every single character you send to it.

How are you observing this "output" ?

 


@sreedharan1196 wrote:

CURRENT OUTPUT :

11:21:33.298 -> ceData?dev=2122001&mr=108&warn=Done"
11:21:33.230 -> OK

 

EXPECTED OUTPUT :

11:21:33.298 -> http://iot.salieabs.in:5003/api/postDeviceData?dev=2122001&mr=108&warn=Done
11:21:33.230 -> OK


So you're missing the first half  (~40 characters) of that string.

Are your buffers big enough?

Again, how are you observing this "output"?