2022-12-14 02:41 AM
Hello, I used SPL2LLConverter tool to migrate a project. The migration went fine but in some of the source files a compatibility_api.h is included which is nowhere to be found. Any clues of what is this file and if it is necessary? If it is, where can I find it to include it myself? I've done some research and there is no information about it.
Thanks
2023-02-15 04:31 AM
Hi @PBlan.1 ,
Sorry for late answer.
I got the confirmation that the file compatibility_api.h will be removed.
I tracked internally the issue for an official fix in a coming release.
Internal ticket number: 145575 (This is an internal tracking number and is not accessible or usable by customers).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.