cancel
Showing results for 
Search instead for 
Did you mean: 

SPI Communication Setup for L3GD20 Sensor on STM32F411VET Board

swati
Associate II

 

Hi Everyone,

I am attempting to communicate with the L3GD20 sensor via SPI communication using the STM32F411VET Board.

Here is my code:

 

#include "main.h"

#include <stdio.h>

#include <string.h>

 

/* USER CODE BEGIN PD */

#define L3GD20_CS_PIN GPIO_PIN_3

#define L3GD20_CS_PORT GPIOE

#define L3GD20_WHO_AM_I 0x0F

#define L3GD20_I_AM 0xD4

 

SPI_HandleTypeDef hspi1;

UART_HandleTypeDef huart2;

 

static uint8_t TxData[2] = {0};

static uint8_t RxData[2] = {0};

 

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_SPI1_Init(void);

static void MX_USART2_UART_Init(void);

uint8_t L3GD20_Init(uint8_t regAddr);

 

int __io_putchar(int ch) {

// Transmit one character to the UART bit by bit

// Transmit one character to the UART

HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);

return ch;

}

 

int main(void)

{

/* USER CODE BEGIN 1 */

 

/* USER CODE END 1 */

 

/* MCU Configuration--------------------------------------------------------*/

 

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

 

/* USER CODE BEGIN Init */

 

/* USER CODE END Init */

 

/* Configure the system clock */

SystemClock_Config();

 

/* USER CODE BEGIN SysInit */

 

/* USER CODE END SysInit */

 

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_SPI1_Init();

MX_USART2_UART_Init();

/* USER CODE BEGIN 2 */

 

/* USER CODE END 2 */

 

/* Infinite loop */

/* USER CODE BEGIN WHILE */

while (1)

{

/* USER CODE END WHILE */

 

/* USER CODE BEGIN 3 */

HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_13);

HAL_Delay(500);

 

uint8_t whoAmIValue = L3GD20_Init(L3GD20_WHO_AM_I); // Assuming WHO_AM_I register is at address 0x0F

 

if (whoAmIValue == L3GD20_I_AM) // Replace with the correct expected value for L2GD20

{

printf("Sensor is connected");

}

else

{

// WHO_AM_I value does not match, there might be a communication issue

// Handle the error, log a message, or take appropriate action

printf("Sensor is not connected");

}

}

/* USER CODE END 3 */

}

 

/**

* @brief System Clock Configuration

* @retval None

*/

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 

/** Configure the main internal regulator output voltage

*/

__HAL_RCC_PWR_CLK_ENABLE();

__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 

/** Initializes the RCC Oscillators according to the specified parameters

* in the RCC_OscInitTypeDef structure.

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

{

Error_Handler();

}

}

 

/**

* @brief SPI1 Initialization Function

* @param None

* @retval None

*/

static void MX_SPI1_Init(void)

{

 

/* USER CODE BEGIN SPI1_Init 0 */

 

/* USER CODE END SPI1_Init 0 */

 

/* USER CODE BEGIN SPI1_Init 1 */

 

/* USER CODE END SPI1_Init 1 */

/* SPI1 parameter configuration*/

hspi1.Instance = SPI1;

hspi1.Init.Mode = SPI_MODE_MASTER;

hspi1.Init.Direction = SPI_DIRECTION_2LINES;

hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;

hspi1.Init.NSS = SPI_NSS_SOFT;

hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;

hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

hspi1.Init.CRCPolynomial = 10;

if (HAL_SPI_Init(&hspi1) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN SPI1_Init 2 */

 

/* USER CODE END SPI1_Init 2 */

 

}

/* USER CODE BEGIN 4 */

uint8_t L3GD20_Init(uint8_t regAddr) {

uint8_t readCommand = regAddr | 0x80;

uint8_t receivedData;

 

// Select the L3GD20 device (if using hardware NSS)

HAL_GPIO_WritePin(L3GD20_CS_PORT, L3GD20_CS_PIN, GPIO_PIN_RESET);

HAL_Delay(50);

 

// Send command to read WHO_AM_I register

if (HAL_SPI_Transmit(&hspi1, &readCommand, 1, HAL_MAX_DELAY) != HAL_OK) {

Error_Handler();

}

 

// Receive data from WHO_AM_I register

if (HAL_SPI_Receive(&hspi1, &receivedData, 1, HAL_MAX_DELAY) != HAL_OK) {

Error_Handler();

}

 

// Deselect the L3GD20 device (if using hardware NSS)

HAL_GPIO_WritePin(L3GD20_CS_PORT, L3GD20_CS_PIN, GPIO_PIN_SET);

 

// Print received data

printf("Received data from register 0x%02X: 0x%02X\n", regAddr, receivedData);

 

return receivedData;

}

I want to start with this sensor but i am receiving

Sensor is not connected Received data from register 0x0F: 0xD3
Sensor is not connected Received data from register 0x0F: 0xD3
Sensor is not connected Received data from register 0x0F: 0xD3
Sensor is not connected Received data from register 0x0F: 0xD3

Can anyone help me identify where I may be wrong?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Unfortunately, the markings for that sheet are not specified in the datasheet.

I would guess it's actually a L3G4200D chip based on the register value. Perhaps there are other differences in the registers which you could examine to find out.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

10 REPLIES 10
TDK
Super User

Perhaps the chip is not what you think it is.

#define WHO_I_AM_L3G4200D 0xD3 /* for L3G4200D */

What hardware is this? Post a high resolution in focus picture of the chip.

 

If you feel a post has answered your question, please click "Accept as Solution".
swati
Associate II

Hi,

I am using STM32F411VET6 and also attaching Images of the controller.

 

Thanks,

IMG_20240213_101241.jpgIMG_20240213_101258.jpgIMG_20240213_102206.jpg

Hi,

is the "CS" pin configured as an output pin? With PullUp?

Your Prescaler for SPI is 2 so you get a >16 MHz on the SPI.

Datasheet says max 10Mhz.

HTH

padawan

 

Hi,

Yes, i configured CS pin as an output with no PullUp,
here is my code snippet

static void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_InitStruct = {0};

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOE_CLK_ENABLE();

__HAL_RCC_GPIOA_CLK_ENABLE();

__HAL_RCC_GPIOD_CLK_ENABLE();

 

/*Configure GPIO pin Output Level */

HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET);

 

/*Configure GPIO pin Output Level */

HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);

 

/*Configure GPIO pin : PE3 */

GPIO_InitStruct.Pin = GPIO_PIN_3;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 

/*Configure GPIO pin : PD14 */

GPIO_InitStruct.Pin = GPIO_PIN_14;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

}


For SPI Configuration

static void MX_SPI1_Init(void)

{

/* SPI1 parameter configuration*/

hspi1.Instance = SPI1;

hspi1.Init.Mode = SPI_MODE_MASTER;

hspi1.Init.Direction = SPI_DIRECTION_2LINES;

hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;

hspi1.Init.NSS = SPI_NSS_SOFT;

hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;

hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

hspi1.Init.CRCPolynomial = 10;

if (HAL_SPI_Init(&hspi1) != HAL_OK)

{

Error_Handler();

}

}



 

TDK
Super User

Unfortunately, the markings for that sheet are not specified in the datasheet.

I would guess it's actually a L3G4200D chip based on the register value. Perhaps there are other differences in the registers which you could examine to find out.

If you feel a post has answered your question, please click "Accept as Solution".

Use this button to properly post source code:

AndrewNeil_0-1707835615337.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi

if i look at 

https://qyriad.github.io/arduino-l3g4200d/html/group__registers.html

is at the bottom of the page

"The chip ID constant value of REG_WHO_AM_I0xd3".

so the reading of your code is correct.

<quote of your code>

"Sensor is not connected Received data from register 0x0F: 0xD3"

</quote of your code> 

hth 

padawan

Thanks for guiding me, i will make sure to use this format in future.

Hi

If you feel a post has answered your question, please click "Accept as Solution".

padawan