2024-03-27 02:54 AM
Hi, I use CubeIDE 12 and compile and load my code with the the green and white 'run debug' button at the top. That works fine but at the end some file from the project pops up and the editor is focus away from the sourcefile to that file. Where/how can I configure this?
THX
Cheers
Detlef
2024-03-27 03:02 AM
Hello @DetlefS
Could you please try to update to last version of the STM32CubeIde.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-27 03:02 AM
This is a well-known issue - nothing you can do about it, I'm afraid:
https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-14-0-gt-old-issue/td-p/612850
@Souhaib MAZHOUD - any update on that "internal ticket 162500" ?
2024-03-27 03:22 AM
Hi, ok, good to know. I only update to a newer version if I'm forced to. Clicking away an unwanted file is too weak a force to update :) .
THX
Cheers
Detlef