2025-02-11 08:43 PM - last edited on 2025-02-12 12:15 AM by SofLit
I am trying to debug the STM32H755 within CUBEIDE but the current segger J-link drivers say that core is not supported. The segger website lists it as supported and it works without issues in their debuggers.
I am wondering if there is a workaround or way to get it working with the CM4 core?
CM7 works as expected.
Thanks.
2025-02-13 01:36 PM
IIRC when you run the updater of J-Flash, it automatically finds J-Link modules (DLLs) installed in other software and updates these. Try it. Chances are it will update your CubeIDE.
2025-02-14 09:33 AM
Hi Pavel, how do I run the J-Flash updater? just running the Stm32cubeide J-Flash program doesn't seem to start any update.
Is the updater in cubeide menus? or is it a program or script in the external tools jlink folder?
Thanks!
2025-02-14 11:53 AM - edited 2025-02-14 12:10 PM
@Ckerl.2 Download and run latest J-Link installer from Segger https://www.segger.com/downloads/jlink/
(this is a bit confusing: the J-Link installer installs a large set of various programs and utilities. Some of them are interesting and useful, others less so).
2025-02-14 12:53 PM - edited 2025-02-14 12:56 PM
Tried this, same behavior when debugging CM4 core, says device not supported and could not verify device.
Then goes to immediate hard fault.
Tried on windows, windows has a JLINKDLLupdater executable.
Wondering how I would get to work with linux, can I just copy over st files with latest segger.