2021-03-10 5:32 AM
Hi. I have some troubles with example.
IDE ver. 1.6
SBSFU ver. 2.4
NUCLEO-H753ZI example
SBSFU now have only SW4STM32 examples. In SW4STM32 IDE this examample build ok, without warnings and errors. Try to convert example to CubeIDE.
Core project build ok, SBSFU project build ok, after that i try to build UserApp project, and i have this error:
arm-none-eabi-gcc -z max-page-size=1 -o "UserApp.elf" @"objects.list" -l:se_interface_app.o -mcpu=cortex-m7 -T"../STM32H753ZITx.ld" --specs=nosys.specs -Wl,-Map="UserApp.map" -Wl,--gc-sections -static -Wl,--start-group -l:se_interface_app.o -Wl,--end-group -L../../../../2_Images_SBSFU/SW4STM32/STM32H753ZI-Nucleo_2_Images_SBSFU/Debug -Xlinker -L ../../../../Linker_Common/SW4STM32 --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
c:\work\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../../2_Images_SBSFU/SW4STM32/STM32H753ZI-Nucleo_2_Images_SBSFU/Debug\se_interface_app.o: in function `SE_APP_GetActiveFwInfo':
(.SE_IF_Code+0x0): multiple definition of `SE_APP_GetActiveFwInfo'; ../../../../2_Images_SBSFU/SW4STM32/STM32H753ZI-Nucleo_2_Images_SBSFU/Debug\se_interface_app.o:(.SE_IF_Code+0x0): first defined here
collect2.exe: error: ld returned 1 exit status
How i can fix this multiply definition? Thank you.
Solved! Go to Solution.
2021-03-11 12:22 AM
2021-03-11 12:22 AM
2021-03-11 3:26 AM
It works. Thank you.