2024-07-15 02:41 AM
Hello STM32 Community,
I am working on a project that involves interfacing a 24-bit RGB display using the LTDC (LCD-TFT Display Controller) with an STM32H753 microcontroller. Despite going through the reference manual and various resources, I am finding it challenging to get the display up and running.
Could anyone share sample code or a detailed guide to properly configure the LTDC peripheral and drive a 24-bit RGB display? Specifically, I am looking for help with:
Any examples, tutorials, or advice from your experience would be greatly appreciated.
2024-07-15 07:20 AM - edited 2024-07-15 07:21 AM
Hello @smj-11 and welcome to the Community 🙂,
I advise you to take a look at AN4861 application note and precisely 7.2 Example: creating a basic graphical application. This section provides an example based on the STM32F746G-DISCO board, describing the steps required to create a basic graphic application using STM32CubeMx. The desired display panel display.
I recommend you to get inspired from this example to create your own project using STM32H753.
I hope this help you.
Thank you for your contribution in STCommunity.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-15 07:27 AM
Perhaps look at STM32H7x3-EVAL(2) boards, those were primarily parallel, not DSI, so should be good examples.
LTDC just funnels to DSIHOST, in those cases, but the frame, rastering, speed was typically nearly identical, and DSI just needs to be at least as fast to funnel into serial stream/lanes.
Timing Parameters, got to read the DISPLAY'S manual data sheet to understand it's expectations and limits.