cancel
Showing results for 
Search instead for 
Did you mean: 

Reverting CubeIDE to previous version (solved)

TJack.2
Associate III

Having upgraded CubeIDE to version 1.17.0 using 'check for updates' and found it didn't work for my project, I tried to go back to version 1.15.1 using the revert button.  After running this, the IDE would not start and give an error message indicating that the ~/.eclipse/com.st.stm32cube.ide.mcu.rcp.product_1.15.1_139064214_linux_gtk_x86_64/configuration/config.ini file had blank filenames.  I found what looked like a complete file at /opt/st/stm32cubeide_1.15.1/configuration/config.ini which I copied to the above location and which then worked OK.

1 REPLY 1
SofLit
ST Employee

Hello @TJack.2 ,

Better to ask a question / describe the issue then add a comment where you provide the solution and accept it as solution.

Thanks

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.