Resurfacing LWIP Configuration Issue with NO_SYS for STM32CubeIDE and FreeRTOS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-10 9:24 AM
As per JimSChen.4 said in the year of 2020, "This question has been asked several times but I have to raise it again". I am stuck on this EXACTLY same issue again.
Board: STM32H757-EVAL
STM32CubeIDE: Version 1.15.1 (Build: 21094_20240412_1041(UTC))
STM32CubeMX version (6.11.1)
STM32Cube FW_H7 V1.11.2
Configuration:
System Core->CORTEX_M7: both CPU DCache and ICache are enabled
Connectivity->ETH->Mode: RMII
FREERTOS_M7: CMSIS_V2
Now the issue is exactly as JimSchen said in this link "STM32CubeMx NO_SYS/With_RTOS option problem with lwip and FREERTOS"
1. LWIP's "Enable" greys out if only Cortex-M7 is selected.
2. When both Cortex-M7 and Cortex-M4 are selected, "Enable" becomes available. However, NO_SYS (OS Awareness) is always "OS Not Used" and unchangeable.
By the way, an old project, created by using STM32CubeMX version (6.8.1) and STM32Cube FW_H7 V1.11.0, does not have this issue. I can still enable LWIP with only Cortex_M7 selected. However, if migrate to the latest Mx and FW, it has the same issue.
 The attached "H757_EVAL_LWIP" is the project with issue, and "ethernet" is my old one without issue.
@Amel NASRI
Solved! Go to Solution.
- Labels:
-
STM32CubeIDE
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-11 6:48 AM
Hello @Leoq ,
Thank you for pointing this out. In fact, this is a known and confirmed issue and it is actively being worked on in internal ticket number 182330 and 178614 and it will be corrected in next revision of CubeMX .
this thread has the same issue Solved: NUCLEO-H755 - ETH configured (Non-RTOS) but LWIP r... - STMicroelectronics Community.
and as a workaround you can proceed by activation of LwIP for booth M7 and M4 and then you can configure it for M7, and you can enable FreeRTOS for M7 only.
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-11 6:48 AM
Hello @Leoq ,
Thank you for pointing this out. In fact, this is a known and confirmed issue and it is actively being worked on in internal ticket number 182330 and 178614 and it will be corrected in next revision of CubeMX .
this thread has the same issue Solved: NUCLEO-H755 - ETH configured (Non-RTOS) but LWIP r... - STMicroelectronics Community.
and as a workaround you can proceed by activation of LwIP for booth M7 and M4 and then you can configure it for M7, and you can enable FreeRTOS for M7 only.
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-11 9:24 AM
Thank you for quick response. The most important is "LWIP->Key Options->Infrastructure - OS Awareness Option/NO_SYS (OS Awareness)" has value of "OS Not Used". This is not changeable !
As a result, the above workaround could not work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-22 4:12 AM
Hello @Leoz ,
The correction of this issue is included in CubeMX 6.12.0 .
Regards