cancel
Showing results for 
Search instead for 
Did you mean: 

Renaming a SMT32CubeIDE project.

LMorr.3
Senior II

I have a project folder named 'myProject' on my hard drive. I want to rename it to 'myProjectOld'. How do I do this in SMT32CubeIDE? I tried using the 'rename' function however it only renames the project in SMT32CubeIDE and not the directory on the hard drive. If I delete 'myProject' from my workspace, close SMT32CubeIDE, rename my directory to 'myProjectOld', and try to 'import' it back into SMT32CubeIDE, nothing happens. It does not appear in my workspace and I see no message of any kind.

Any ideas?

2 REPLIES 2
LMorr.3
Senior II

Update: I was able to rename a project by first using the 'rename' feature in SMT32CubeIDE to rename it to 'myProjectOld', and I then 'deleted' that project from the workspace. ( kept files on local drive ) I closed SMT32CubeIDE and renamed the directory to 'myProjectOld'. I opened SMT32CubeIDE and used the 'import' feature to load my renamed project into my workspace as 'myProjectOld'. I was able to create a new project named 'myProject'.

Not sure if this is the correct way to rename.

Yes, this is one of correct ways to rename. Should be safe.

Closing CubeIDE is not required when the project is closed and unloaded.