2022-04-13 07:36 AM
I have a project folder named 'myProject' on my hard drive. I want to rename it to 'myProjectOld'. How do I do this in SMT32CubeIDE? I tried using the 'rename' function however it only renames the project in SMT32CubeIDE and not the directory on the hard drive. If I delete 'myProject' from my workspace, close SMT32CubeIDE, rename my directory to 'myProjectOld', and try to 'import' it back into SMT32CubeIDE, nothing happens. It does not appear in my workspace and I see no message of any kind.
Any ideas?
2022-04-13 07:56 AM
Update: I was able to rename a project by first using the 'rename' feature in SMT32CubeIDE to rename it to 'myProjectOld', and I then 'deleted' that project from the workspace. ( kept files on local drive ) I closed SMT32CubeIDE and renamed the directory to 'myProjectOld'. I opened SMT32CubeIDE and used the 'import' feature to load my renamed project into my workspace as 'myProjectOld'. I was able to create a new project named 'myProject'.
Not sure if this is the correct way to rename.
2022-04-13 04:25 PM
Yes, this is one of correct ways to rename. Should be safe.
Closing CubeIDE is not required when the project is closed and unloaded.