cancel
Showing results for 
Search instead for 
Did you mean: 

rand()

eunni
Associate III

Hi,

I want to use random number.

But, the same random number is generated each time it is run.

When I debug the code below, W change with the same pattern every time I debug.

 

What's the problem and is there any solution to make random number which is not depend on the order? 

 

 

/* USER CODE BEGIN 0 */

double uniform_rand(){

return (double)rand()/((double)RAND_MAX + 1);

}

/* USER CODE END 0 */

 

 

int main(void) {

/* USER CODE BEGIN 2 */

srand(time(NULL));

/* USER CODE END 2 */

 

while {

W = uniform_rand();

}

}

1 ACCEPTED SOLUTION

Accepted Solutions

I'm using 2 kinds of board for i2c.

One is U575ZI-Q for master and the other is L432KC for slave.


Hello,

The two devices feature RNG (random number generator) as shown in their respective DS:

SofLit_0-1714645265840.png

You can inspire from one of the examples of RNG. Example:

https://github.com/STMicroelectronics/STM32CubeL4/tree/master/Projects/NUCLEO-L432KC/Examples/RNG/RNG_MultiRNG

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

View solution in original post

8 REPLIES 8
SofLit
ST Employee

Hello,

What product you're using so you can use RNG peripheral instead of that "rand" library?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

sorry but I can't understand what you're saying...

isn't it "rand" library?

 

srand(time(NULL));

rand() from stdlib.h

What MCU part number are you using?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

Need to seed it better.

Is there a clock or anything behind time() ? There'd need to be some association with the RTC and it would need to be running.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Yes I use rand() function from stdlib.h

 

I'm using 2 kinds of board for i2c.

One is U575ZI-Q for master and the other is L432KC for slave.

I didn't use anything according to the clock.

Is there any recommandation to make better seed?

 

srand(time(NULL)); <----------- I think it change seed every single second

That supposes time() is working and there's anything making it tick.

In embedded you'd actually need to facilitate this.

You should confirm that it is working as you imagine.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I'm using 2 kinds of board for i2c.

One is U575ZI-Q for master and the other is L432KC for slave.


Hello,

The two devices feature RNG (random number generator) as shown in their respective DS:

SofLit_0-1714645265840.png

You can inspire from one of the examples of RNG. Example:

https://github.com/STMicroelectronics/STM32CubeL4/tree/master/Projects/NUCLEO-L432KC/Examples/RNG/RNG_MultiRNG

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.